<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8M: PCIe port as SGMII Interface possible? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1277213#M174083</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158536"&gt;@sergeyan&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; it depends on applications - if heatsink or /and fan are needed. &lt;BR /&gt;Thermal estimations, using thermal resistance data in the Datasheet&lt;BR /&gt;or thermal models, should be performed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Sun, 16 May 2021 08:24:16 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2021-05-16T08:24:16Z</dc:date>
    <item>
      <title>IMX8M: PCIe port as SGMII Interface possible?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276359#M174004</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Is it possible to configure the PCIe port as a SGMII Interface and connect a PHY to it to establish a connection to the Etnernet?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 10:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276359#M174004</guid>
      <dc:creator>sergeyan</dc:creator>
      <dc:date>2021-05-13T10:14:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M: PCIe port as SGMII Interface possible?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276388#M174008</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158536"&gt;@sergeyan&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; alas, no - it is not possible to configure the PCIe port as a SGMII Interface.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 11:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276388#M174008</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-05-13T11:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M: PCIe port as SGMII Interface possible?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276395#M174011</link>
      <description>&lt;P&gt;Hello, Yuri!&lt;/P&gt;&lt;P&gt;That is, the internal content of the PCIe port IMX8* differs from that of the SerDes ports of other CPUs such as LS1043A or S32G?&lt;/P&gt;&lt;P&gt;Then is it possible to use an external Ethernet bridge with the PCIe interface (LAN7430 "Microchip")?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 12:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276395#M174011</guid>
      <dc:creator>sergeyan</dc:creator>
      <dc:date>2021-05-13T12:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M: PCIe port as SGMII Interface possible?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276736#M174040</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158536"&gt;@sergeyan&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; i.MX devices do not support the SerDes.&lt;BR /&gt;As for external Ethernet bridge with the PCIe interface - it is possible. &lt;BR /&gt;Note: customers should adapt Linux driver(s), if needed.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Fri, 14 May 2021 05:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276736#M174040</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-05-14T05:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M: PCIe port as SGMII Interface possible?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276766#M174042</link>
      <description>&lt;P&gt;Hello, Yuri&lt;/P&gt;&lt;P&gt;It's a pity, we bought EVAL Board for imx8m, but we had to choose EVAL for S32G2.&lt;/P&gt;&lt;P&gt;We need a "warm" (1-2W) (possibly without a heatsink) CPU with three or four MACs.&lt;/P&gt;&lt;P&gt;Another question: is it possible to choose a power profile CPU by standard means for work without a heatsink and fans (only on a board) on the S32G2, IMX8M?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 14 May 2021 05:47:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1276766#M174042</guid>
      <dc:creator>sergeyan</dc:creator>
      <dc:date>2021-05-14T05:47:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M: PCIe port as SGMII Interface possible?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1277213#M174083</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158536"&gt;@sergeyan&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; it depends on applications - if heatsink or /and fan are needed. &lt;BR /&gt;Thermal estimations, using thermal resistance data in the Datasheet&lt;BR /&gt;or thermal models, should be performed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Sun, 16 May 2021 08:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-PCIe-port-as-SGMII-Interface-possible/m-p/1277213#M174083</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-05-16T08:24:16Z</dc:date>
    </item>
  </channel>
</rss>