<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6DL MMU setup in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-MMU-setup/m-p/1275830#M173947</link>
    <description>&lt;P&gt;Hello I've starting working with the IMX6 dual lite board. My company runs all our applications with a bare metal implementation. I've gotten both core running but core 1 is extremely slow due to MMU not being set up. If I just try and copy what was done with the single core the processor crashes or I get undefined behavior. Does anyone know how to correctly setup the memory to separate core 0 from core 1 and also have a shared memory region. We would need to run this in AMP implantation as well.&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Micah&lt;/P&gt;</description>
    <pubDate>Wed, 12 May 2021 18:06:09 GMT</pubDate>
    <dc:creator>mjrudy</dc:creator>
    <dc:date>2021-05-12T18:06:09Z</dc:date>
    <item>
      <title>iMX6DL MMU setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-MMU-setup/m-p/1275830#M173947</link>
      <description>&lt;P&gt;Hello I've starting working with the IMX6 dual lite board. My company runs all our applications with a bare metal implementation. I've gotten both core running but core 1 is extremely slow due to MMU not being set up. If I just try and copy what was done with the single core the processor crashes or I get undefined behavior. Does anyone know how to correctly setup the memory to separate core 0 from core 1 and also have a shared memory region. We would need to run this in AMP implantation as well.&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Micah&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 18:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-MMU-setup/m-p/1275830#M173947</guid>
      <dc:creator>mjrudy</dc:creator>
      <dc:date>2021-05-12T18:06:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DL MMU setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-MMU-setup/m-p/1276031#M173962</link>
      <description>&lt;P&gt;Hi Micah&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try below patch&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enabling-MMU-and-Caches-on-i-MX6-Series-Platform-SDK/ta-p/1108712" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enabling-MMU-and-Caches-on-i-MX6-Series-Platform-SDK/ta-p/1108712&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 00:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-MMU-setup/m-p/1276031#M173962</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-05-13T00:31:43Z</dc:date>
    </item>
  </channel>
</rss>