<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX6 Development Environment Setup</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Development-Environment-Setup/m-p/1275304#M173898</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is this app note the most up to date guide for setting up a cross-compiling/cross-debugging environment for the i.MX family using Eclipse?&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3870.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN3870.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It seems little old and just wondered if there is anything more current. We're using i.MX6ULL EVK. And is LTIB still a recommended tool to use?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 12 May 2021 03:23:09 GMT</pubDate>
    <dc:creator>ddebaun</dc:creator>
    <dc:date>2021-05-12T03:23:09Z</dc:date>
    <item>
      <title>i.MX6 Development Environment Setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Development-Environment-Setup/m-p/1275304#M173898</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is this app note the most up to date guide for setting up a cross-compiling/cross-debugging environment for the i.MX family using Eclipse?&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3870.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN3870.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It seems little old and just wondered if there is anything more current. We're using i.MX6ULL EVK. And is LTIB still a recommended tool to use?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 03:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Development-Environment-Setup/m-p/1275304#M173898</guid>
      <dc:creator>ddebaun</dc:creator>
      <dc:date>2021-05-12T03:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Development Environment Setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Development-Environment-Setup/m-p/1275509#M173919</link>
      <description>&lt;P&gt;Do not recommend to use the LTIB, now we are using the yocto. You can download the new BSP here &lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;For the &lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Eclipse IDE for Yocto you can refer to &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-up-the-Eclipse-IDE-for-Yocto-Application-Development/ta-p/1110480" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-up-the-Eclipse-IDE-for-Yocto-Application-Development/ta-p/1110480&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 09:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Development-Environment-Setup/m-p/1275509#M173919</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-05-12T09:16:49Z</dc:date>
    </item>
  </channel>
</rss>