<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: 2 stop bits</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231143#M17377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Be sure you set termios c_cflag with CSTOPB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 26 Oct 2013 09:15:39 GMT</pubDate>
    <dc:creator>raymondwang</dc:creator>
    <dc:date>2013-10-26T09:15:39Z</dc:date>
    <item>
      <title>2 stop bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231142#M17376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;We have an application that requires serial communications with a peripheral, and this peripheral requires us to send out the data stream with 2 stop bits, however it sends in a data stream with only 1 stop bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;The data sheet specifically states that when the "2 stop bit" configuration bit is set in the uart control register, the receiver will NOT look for 2 stop bits as a condition on incoming data. However, all our investigations show this is not true, and we are getting bad data and framing errors on input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Is this a h/w issue (or a typo in the data sheet)?&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Can it be corrected with firmware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;We are running linux on this platform&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Thanks, Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2013 23:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231142#M17376</guid>
      <dc:creator>adrianc</dc:creator>
      <dc:date>2013-10-24T23:32:16Z</dc:date>
    </item>
    <item>
      <title>Re: 2 stop bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231143#M17377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Be sure you set termios c_cflag with CSTOPB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Oct 2013 09:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231143#M17377</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2013-10-26T09:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: 2 stop bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231144#M17378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is precisely when that bit is set that we have the problems:&lt;/P&gt;&lt;P&gt;outgoing data has the 2 stop bits&lt;/P&gt;&lt;P&gt;incoming data does not, however the uart expects it to have 2 stop bits, whereas our expectation is that it should not (cf data sheet)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Oct 2013 23:25:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231144#M17378</guid>
      <dc:creator>adrianc</dc:creator>
      <dc:date>2013-10-27T23:25:23Z</dc:date>
    </item>
    <item>
      <title>Re: 2 stop bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231145#M17379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please mark this issue as answered.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2013 02:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231145#M17379</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2013-10-29T02:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: 2 stop bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231146#M17380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The UART can be configured as a whole, i.e. settings for the TX and RX sides are common, or the TX and RX sections can be configured individually. Thus setting different stop bit, parity, data lengths for each section. By default the Linux drivers set the UART as a whole, the following sequence inserted into the serial drivers allow the application to behave as we want, 2 stop bits outgoing, 1 stop bit incoming:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1st line puts the same configuration in the control registers for TX and RX. The global line control register becomes the RX line control register, the 2 line control registers is used for the TX section.&lt;/P&gt;&lt;P&gt;2nd line tells the UART to apply the 2 control registers for settings, 1 for TX 1 for RX&lt;/P&gt;&lt;P&gt;3rd line changes the settings in the TX section of the UART.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-top: 10px; color: #333333; font-family: Arial, sans-serif; font-size: 14px; background-color: #f0f0f0;"&gt;1. Copy the HW_UARTAPP_LINECTRL register into the HW_UARTAPP_LINECTRL2 regfister&lt;BR /&gt;2. Set the USE_LCR2 bit in the HW_UARTAPP_CTRL2 register.&lt;BR /&gt;3. Set the STP2 bit in the HW_UARTAPP_LINECTRL2 register.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2013 23:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2-stop-bits/m-p/231146#M17380</guid>
      <dc:creator>adrianc</dc:creator>
      <dc:date>2013-10-29T23:16:29Z</dc:date>
    </item>
  </channel>
</rss>