<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTwo Separate MIPI-CSI Input Streams for Stereo Vision</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Two-Separate-MIPI-CSI-Input-Streams-for-Stereo-Vision/m-p/1273306#M173704</link>
    <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I have a question for you about the i.MX 8M Plus ISP capability that I was not able to find an answer to by reading the i.MX 8M Plus documentation.&lt;/P&gt;&lt;P&gt;We have our stereo vision cameras already working with the NXP development board, but we want to plan accordingly for finalization of a camera adapter board for our own system.&lt;/P&gt;&lt;P&gt;When targeting our system, we will have access to a camera on a x4 MIPI CSI lane and another camera on a x2 MIPI CSI lane.&amp;nbsp; I wanted to verify whether the integrated ISP could support simultaneous input from two separate camera input streams for a stereo vision application.&amp;nbsp; Is this possible with the support in place for the ISP today?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Kevin&lt;/P&gt;</description>
    <pubDate>Fri, 07 May 2021 00:42:00 GMT</pubDate>
    <dc:creator>kevin_keryk</dc:creator>
    <dc:date>2021-05-07T00:42:00Z</dc:date>
    <item>
      <title>Two Separate MIPI-CSI Input Streams for Stereo Vision</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-Separate-MIPI-CSI-Input-Streams-for-Stereo-Vision/m-p/1273306#M173704</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I have a question for you about the i.MX 8M Plus ISP capability that I was not able to find an answer to by reading the i.MX 8M Plus documentation.&lt;/P&gt;&lt;P&gt;We have our stereo vision cameras already working with the NXP development board, but we want to plan accordingly for finalization of a camera adapter board for our own system.&lt;/P&gt;&lt;P&gt;When targeting our system, we will have access to a camera on a x4 MIPI CSI lane and another camera on a x2 MIPI CSI lane.&amp;nbsp; I wanted to verify whether the integrated ISP could support simultaneous input from two separate camera input streams for a stereo vision application.&amp;nbsp; Is this possible with the support in place for the ISP today?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Kevin&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 00:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-Separate-MIPI-CSI-Input-Streams-for-Stereo-Vision/m-p/1273306#M173704</guid>
      <dc:creator>kevin_keryk</dc:creator>
      <dc:date>2021-05-07T00:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: Two Separate MIPI-CSI Input Streams for Stereo Vision</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-Separate-MIPI-CSI-Input-Streams-for-Stereo-Vision/m-p/1273628#M173731</link>
      <description>&lt;P&gt;yes, imx8mp can support dual camera via different ISP , you can refer to the basler dts file as reference, which supports two 4-lanes basler via dual ISP&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-dual-basler.dts?h=imx_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-dual-basler.dts?h=imx_5.4.70_2.3.0&lt;/A&gt;"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 09:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-Separate-MIPI-CSI-Input-Streams-for-Stereo-Vision/m-p/1273628#M173731</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-05-07T09:52:53Z</dc:date>
    </item>
  </channel>
</rss>