<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6dl flexcan performance</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6dl-flexcan-performance/m-p/1272383#M173635</link>
    <description>&lt;P&gt;Hi All ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have one performance issue on flexcan application test&lt;/P&gt;&lt;P&gt;preconditions:&lt;/P&gt;&lt;P&gt;CAN Baud:125Kbps&lt;/P&gt;&lt;P&gt;NODE A:&lt;/P&gt;&lt;P&gt;i am using socketcan FD.read and write for&amp;nbsp; transmitting and receiving10 CAN frames with each frame data length 16 bytes. with delay of 100 ms sec, then next Frame will be sent&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;10 Frame consecutive write also success&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;here all the can send are success&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;but receiving node B:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;few last &lt;STRONG&gt;8/9th FRAME&amp;nbsp; are not read&lt;/STRONG&gt;, with following&amp;nbsp; node B CAN status&lt;/P&gt;&lt;P&gt;shell ifconfig can0&lt;BR /&gt;can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00&lt;BR /&gt;UP RUNNING NOARP MTU:16 Metric:1&lt;BR /&gt;RX packets:19263 errors:2 dropped:0 overruns:0 frame:2&lt;BR /&gt;TX packets:4028 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:10&lt;BR /&gt;RX bytes:147976 (144.5 KiB) TX bytes:8064 (7.8 KiB)&lt;BR /&gt;Interrupt:35&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to improvise,&lt;/P&gt;&lt;P&gt;1. i added a delay in Node A every CAN frame by delay 20 ms with usleep,&lt;/P&gt;&lt;P&gt;2. Node B works neatly reads all frames successfully&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;anyone faced issue, i am using standard linux kernel 4.19 yocto build&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 05 May 2021 18:37:44 GMT</pubDate>
    <dc:creator>starimx</dc:creator>
    <dc:date>2021-05-05T18:37:44Z</dc:date>
    <item>
      <title>imx6dl flexcan performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6dl-flexcan-performance/m-p/1272383#M173635</link>
      <description>&lt;P&gt;Hi All ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have one performance issue on flexcan application test&lt;/P&gt;&lt;P&gt;preconditions:&lt;/P&gt;&lt;P&gt;CAN Baud:125Kbps&lt;/P&gt;&lt;P&gt;NODE A:&lt;/P&gt;&lt;P&gt;i am using socketcan FD.read and write for&amp;nbsp; transmitting and receiving10 CAN frames with each frame data length 16 bytes. with delay of 100 ms sec, then next Frame will be sent&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;10 Frame consecutive write also success&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;here all the can send are success&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;but receiving node B:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;few last &lt;STRONG&gt;8/9th FRAME&amp;nbsp; are not read&lt;/STRONG&gt;, with following&amp;nbsp; node B CAN status&lt;/P&gt;&lt;P&gt;shell ifconfig can0&lt;BR /&gt;can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00&lt;BR /&gt;UP RUNNING NOARP MTU:16 Metric:1&lt;BR /&gt;RX packets:19263 errors:2 dropped:0 overruns:0 frame:2&lt;BR /&gt;TX packets:4028 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:10&lt;BR /&gt;RX bytes:147976 (144.5 KiB) TX bytes:8064 (7.8 KiB)&lt;BR /&gt;Interrupt:35&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to improvise,&lt;/P&gt;&lt;P&gt;1. i added a delay in Node A every CAN frame by delay 20 ms with usleep,&lt;/P&gt;&lt;P&gt;2. Node B works neatly reads all frames successfully&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;anyone faced issue, i am using standard linux kernel 4.19 yocto build&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 18:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6dl-flexcan-performance/m-p/1272383#M173635</guid>
      <dc:creator>starimx</dc:creator>
      <dc:date>2021-05-05T18:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx6dl flexcan performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6dl-flexcan-performance/m-p/1272781#M173660</link>
      <description>&lt;P&gt;Hi Anith&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;may be recommended to test this case with two Sabre SD boards and Demo Image&lt;/P&gt;
&lt;P&gt;&lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_MX6QDLSOLOX&amp;amp;appType=license" target="_blank" rel="noopener"&gt;i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6SoloX&lt;/A&gt;​&lt;/P&gt;
&lt;P&gt;use simple can test:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/test/can/doc/FSL-UT-CAN-003.txt?h=imx_4.19.35_1.0.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/test/can/doc/FSL-UT-CAN-003.txt?h=imx_4.19.35_1.0.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 06 May 2021 07:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6dl-flexcan-performance/m-p/1272781#M173660</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-05-06T07:24:44Z</dc:date>
    </item>
  </channel>
</rss>