<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8 - LPDDR4 RPA tool + DDR Tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271992#M173599</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186168"&gt;@NathanSmith&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; I meant the following:&lt;/P&gt;
&lt;P&gt;4.4 Run DDR Calibration and generate DDR initial code&lt;/P&gt;
&lt;P&gt;Please follow chapter 3 to run DDR calibration and stress test &lt;BR /&gt;with your board specific script. If there is no problem, Congratulations,&lt;BR /&gt;you can generate DDR initial code now. In initial DDR script, RPA tool &lt;BR /&gt;always use NXP reference board related parameters. Your board design and &lt;BR /&gt;manufacturing technology are different from NXP reference board, and board &lt;BR /&gt;related parameters may differ from initial DDR script. If DDR calibration failed,&lt;BR /&gt;you can try to modify following DDR parameters in script.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;TrainInfo&lt;/STRONG&gt; This parameter controls DDR training debug message. The default value is 0xc8, &lt;BR /&gt;which means only display stage completion message. You can change to 0x05 to get detailed&lt;BR /&gt;debug message when DDR training failed. &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;ODTImpedance&lt;/STRONG&gt; Desired ODT impedance in Ohm. Valid values for DDR4=240,120,80,60,40. &lt;BR /&gt;Valid values for DDR3L=high-impedance,120,60,40. Valid values for LPDDR4=240,120,80,60,40 &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;TxImpedance&lt;/STRONG&gt; Write Driver Impedance for DQ/DQS in ohm (Valid values for all DDR type= 240, 120, &lt;BR /&gt;80, 60, 48, 40, 34) &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;ATxImpedance&lt;/STRONG&gt; Write Driver Impedance for Address/Command (AC) bus in ohm (Valid values for all &lt;BR /&gt;DDR type = 120, 60, 40, 30, 24, 20) &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;PhyVref&lt;/STRONG&gt; This parameter is used for 1D training process. You can refer to DDR datasheet for &lt;BR /&gt;detailed meaning. &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Mode Registers (MR0~MR22)&lt;/STRONG&gt; There are different meanings for different DDR types. Please refer &lt;BR /&gt;to DDR datasheet for detailed information. Remember don’t manually modify the Mode Registers. &lt;BR /&gt;Instead, please modify Mode Registers in RPA tool. Because there may be other parameters related&lt;BR /&gt;to the Mode Registers.&lt;/P&gt;
&lt;P&gt;Note - no more parameters, available for customers.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Wed, 05 May 2021 04:22:39 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2021-05-05T04:22:39Z</dc:date>
    <item>
      <title>iMX8 - LPDDR4 RPA tool + DDR Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1270937#M173477</link>
      <description>&lt;P&gt;I have a question regarding the ODTImpedance (line 613 of Register Configuration, RPA tool V28).&amp;nbsp; This appears to be an input to the calibration / training algorithms in the DDR tool and not a direct register configuration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this parameter for the desired termination of the command bus (CA, CS) or the desired termination of the data bus (DQ, DM)?&lt;/P&gt;&lt;P&gt;What effect does this parameter have on the calibration process and training process?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 15:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1270937#M173477</guid>
      <dc:creator>NathanSmith</dc:creator>
      <dc:date>2021-04-30T15:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 - LPDDR4 RPA tool + DDR Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271578#M173550</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186168"&gt;@NathanSmith&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P class="Normal"&gt;&lt;SPAN class="tm5"&gt;&amp;nbsp; Please use section 4.4 (Run DDR Calibration and generate DDR initial code) &lt;BR /&gt;of “MSCALE_DDR_Tool_User_Guide.pdf”.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P class="Normal"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="Normal"&gt;&lt;SPAN class="tm5"&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467?attachment-id=110481" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467?attachment-id=110481 &lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P class="Normal"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="Normal"&gt;&lt;SPAN class="tm5"&gt;Summary Page:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P class="Normal"&gt;&lt;SPAN class="tm5"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="tm5"&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 05:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271578#M173550</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-05-04T05:47:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 - LPDDR4 RPA tool + DDR Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271691#M173563</link>
      <description>&lt;P&gt;Thanks.&amp;nbsp; We have been through the DDR tool documentation (Rev V2.0.0) and the developers guide (Rev 1) and it seems ambiguous to which bus this parameter is referring too.&amp;nbsp; I could not find any reference to this parameter on the Summary page you referenced (this is where we downloaded all the tools from).&amp;nbsp; It does not give guidance for this parameter.&amp;nbsp; The impedance controls are bus independent on the LPDDR4 device so I would expect this is referring to the data bus or the command bus but not both at the same time.&amp;nbsp; It does not make mention to how or what this parameter is controlling in the calibration process.&amp;nbsp; We were expecting a clearer definition or better guidance for the parameter for such an important part of the design and verification process.&amp;nbsp; The other parameters are more clearly defined.&lt;/P&gt;&lt;P&gt;Through experimentation I have observed the current on the 1.1V DRAM supply change with this parameter.&amp;nbsp; Is the method to simply guess / tune the value to the lower power consumption while still passing the stress tests across the operating temperature range?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 11:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271691#M173563</guid>
      <dc:creator>NathanSmith</dc:creator>
      <dc:date>2021-05-04T11:49:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 - LPDDR4 RPA tool + DDR Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271992#M173599</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186168"&gt;@NathanSmith&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; I meant the following:&lt;/P&gt;
&lt;P&gt;4.4 Run DDR Calibration and generate DDR initial code&lt;/P&gt;
&lt;P&gt;Please follow chapter 3 to run DDR calibration and stress test &lt;BR /&gt;with your board specific script. If there is no problem, Congratulations,&lt;BR /&gt;you can generate DDR initial code now. In initial DDR script, RPA tool &lt;BR /&gt;always use NXP reference board related parameters. Your board design and &lt;BR /&gt;manufacturing technology are different from NXP reference board, and board &lt;BR /&gt;related parameters may differ from initial DDR script. If DDR calibration failed,&lt;BR /&gt;you can try to modify following DDR parameters in script.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;TrainInfo&lt;/STRONG&gt; This parameter controls DDR training debug message. The default value is 0xc8, &lt;BR /&gt;which means only display stage completion message. You can change to 0x05 to get detailed&lt;BR /&gt;debug message when DDR training failed. &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;ODTImpedance&lt;/STRONG&gt; Desired ODT impedance in Ohm. Valid values for DDR4=240,120,80,60,40. &lt;BR /&gt;Valid values for DDR3L=high-impedance,120,60,40. Valid values for LPDDR4=240,120,80,60,40 &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;TxImpedance&lt;/STRONG&gt; Write Driver Impedance for DQ/DQS in ohm (Valid values for all DDR type= 240, 120, &lt;BR /&gt;80, 60, 48, 40, 34) &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;ATxImpedance&lt;/STRONG&gt; Write Driver Impedance for Address/Command (AC) bus in ohm (Valid values for all &lt;BR /&gt;DDR type = 120, 60, 40, 30, 24, 20) &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;PhyVref&lt;/STRONG&gt; This parameter is used for 1D training process. You can refer to DDR datasheet for &lt;BR /&gt;detailed meaning. &lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Mode Registers (MR0~MR22)&lt;/STRONG&gt; There are different meanings for different DDR types. Please refer &lt;BR /&gt;to DDR datasheet for detailed information. Remember don’t manually modify the Mode Registers. &lt;BR /&gt;Instead, please modify Mode Registers in RPA tool. Because there may be other parameters related&lt;BR /&gt;to the Mode Registers.&lt;/P&gt;
&lt;P&gt;Note - no more parameters, available for customers.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 04:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-LPDDR4-RPA-tool-DDR-Tool/m-p/1271992#M173599</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-05-05T04:22:39Z</dc:date>
    </item>
  </channel>
</rss>