<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック[I.MX6ULL] Mfgtool(Linux version) downloading fail.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Mfgtool-Linux-version-downloading-fail/m-p/1271984#M173596</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I tried to download and burn images to imx6ull under Linux through both mfgtool2 and UUU upon which some problems encountered as describled below.&lt;/P&gt;&lt;P&gt;1.mfgtool2 (mfgtoolcli) error[21]&lt;/P&gt;&lt;P&gt;2.UUU downloading stuck&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Building Env Info:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MX6ULL kernel version:4.1.15&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Build env: Ubuntu 20.04&lt;/LI&gt;&lt;LI&gt;Some hardware have been modified from board imx6ull14x14evk(mostly small type change for ddr3 and nand/emmc）&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Specifics.&lt;/P&gt;&lt;P&gt;My employer designed a product using IMX6ULL for industrial base station use.&amp;nbsp; I have already finished building and compiling&amp;nbsp; procedure. I took use of mfgtool2 under Windows7 before and it worked,but for now we want to finish building and downloading procedure both under Linux env.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First, I tried .sh scrpit in &lt;FONT color="#00CCFF"&gt;L4.1.15_2.0.0-ga_mfg-tools&lt;/FONT&gt; branch, all VBscript and cfg same as they are in Windows7, I tried 'linux-runvbs' and also 'linux-cvbs' later, terminal all shows:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 21&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After that, I fetched new mfgtool(UUU) from ’&lt;A href="https://github.com/NXPmicro/mfgtools.git'" target="_blank"&gt;&lt;FONT color="#00CCFF"&gt;https://github.com/NXPmicro/mfgtools.git&lt;/FONT&gt;'&lt;/A&gt;&amp;nbsp;and also&amp;nbsp;&lt;FONT color="#00CCFF"&gt;LF_v5.10_1.0.0_images_IMX6UL7D.zip&lt;FONT color="#333333"&gt; for image.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;After building uuu, I replace some bootloader&amp;amp;image name in '&lt;EM&gt;example_kernel_emmc.uuu&lt;/EM&gt;', the command I put in cmdline is like '&lt;EM&gt;uuu example_kernel_emmc.uuu&lt;/EM&gt;', but it keeps showing message like below.(the bar keep moving from 0% to 100% ,and some uboot message can be detect from LCD same time.Firmware kept untouched)&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-6-g0ecc166&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;Success 0 Failure 0&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;1:9 1/ 1 [=================100%=================] SDP: boot -f u-boot-imx6ull14x14evk_emmc&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;My question are as below.&lt;/P&gt;&lt;P&gt;1.What is the right procedure for burning images to IMX6ULL through UUU tool? Does my hardware change have influence on that?&lt;/P&gt;&lt;P&gt;2.Would mfgtool2(mfgtoolcli) work properly? or where can I find the source code just for downloading under LinuxOS.&lt;/P&gt;&lt;P&gt;Tks for your kindly help in advance. Looking forward to your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 05 May 2021 03:44:15 GMT</pubDate>
    <dc:creator>zzw</dc:creator>
    <dc:date>2021-05-05T03:44:15Z</dc:date>
    <item>
      <title>[I.MX6ULL] Mfgtool(Linux version) downloading fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Mfgtool-Linux-version-downloading-fail/m-p/1271984#M173596</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I tried to download and burn images to imx6ull under Linux through both mfgtool2 and UUU upon which some problems encountered as describled below.&lt;/P&gt;&lt;P&gt;1.mfgtool2 (mfgtoolcli) error[21]&lt;/P&gt;&lt;P&gt;2.UUU downloading stuck&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Building Env Info:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MX6ULL kernel version:4.1.15&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Build env: Ubuntu 20.04&lt;/LI&gt;&lt;LI&gt;Some hardware have been modified from board imx6ull14x14evk(mostly small type change for ddr3 and nand/emmc）&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Specifics.&lt;/P&gt;&lt;P&gt;My employer designed a product using IMX6ULL for industrial base station use.&amp;nbsp; I have already finished building and compiling&amp;nbsp; procedure. I took use of mfgtool2 under Windows7 before and it worked,but for now we want to finish building and downloading procedure both under Linux env.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First, I tried .sh scrpit in &lt;FONT color="#00CCFF"&gt;L4.1.15_2.0.0-ga_mfg-tools&lt;/FONT&gt; branch, all VBscript and cfg same as they are in Windows7, I tried 'linux-runvbs' and also 'linux-cvbs' later, terminal all shows:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 21&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After that, I fetched new mfgtool(UUU) from ’&lt;A href="https://github.com/NXPmicro/mfgtools.git'" target="_blank"&gt;&lt;FONT color="#00CCFF"&gt;https://github.com/NXPmicro/mfgtools.git&lt;/FONT&gt;'&lt;/A&gt;&amp;nbsp;and also&amp;nbsp;&lt;FONT color="#00CCFF"&gt;LF_v5.10_1.0.0_images_IMX6UL7D.zip&lt;FONT color="#333333"&gt; for image.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;After building uuu, I replace some bootloader&amp;amp;image name in '&lt;EM&gt;example_kernel_emmc.uuu&lt;/EM&gt;', the command I put in cmdline is like '&lt;EM&gt;uuu example_kernel_emmc.uuu&lt;/EM&gt;', but it keeps showing message like below.(the bar keep moving from 0% to 100% ,and some uboot message can be detect from LCD same time.Firmware kept untouched)&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-6-g0ecc166&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;Success 0 Failure 0&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;1:9 1/ 1 [=================100%=================] SDP: boot -f u-boot-imx6ull14x14evk_emmc&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;My question are as below.&lt;/P&gt;&lt;P&gt;1.What is the right procedure for burning images to IMX6ULL through UUU tool? Does my hardware change have influence on that?&lt;/P&gt;&lt;P&gt;2.Would mfgtool2(mfgtoolcli) work properly? or where can I find the source code just for downloading under LinuxOS.&lt;/P&gt;&lt;P&gt;Tks for your kindly help in advance. Looking forward to your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 03:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Mfgtool-Linux-version-downloading-fail/m-p/1271984#M173596</guid>
      <dc:creator>zzw</dc:creator>
      <dc:date>2021-05-05T03:44:15Z</dc:date>
    </item>
    <item>
      <title>Re: [I.MX6ULL] Mfgtool(Linux version) downloading fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Mfgtool-Linux-version-downloading-fail/m-p/1271990#M173597</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to follow steps provided on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX6DP-MfgTool-Stuck-at-Loading-uboot/m-p/1254217#M171787" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX6DP-MfgTool-Stuck-at-Loading-uboot/m-p/1254217#M171787&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 04:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Mfgtool-Linux-version-downloading-fail/m-p/1271990#M173597</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-05-05T04:17:28Z</dc:date>
    </item>
  </channel>
</rss>