<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SCFW API included in Linux Kernel 5.4.24?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-API-included-in-Linux-Kernel-5-4-24/m-p/1271719#M173570</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I see that inside the imx-scfw-porting-kit there is a scfw-export-linux folder with some APIs to be called by the kernel. What i don't understand is: do i need to move these files inside the linux-imx v5.4.24? Or are they already present?&lt;/P&gt;&lt;P&gt;For instance, what if i want to create/modify a partition for HW access?&lt;/P&gt;</description>
    <pubDate>Tue, 04 May 2021 13:41:25 GMT</pubDate>
    <dc:creator>lorenzo_giraudi</dc:creator>
    <dc:date>2021-05-04T13:41:25Z</dc:date>
    <item>
      <title>SCFW API included in Linux Kernel 5.4.24?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-API-included-in-Linux-Kernel-5-4-24/m-p/1271719#M173570</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I see that inside the imx-scfw-porting-kit there is a scfw-export-linux folder with some APIs to be called by the kernel. What i don't understand is: do i need to move these files inside the linux-imx v5.4.24? Or are they already present?&lt;/P&gt;&lt;P&gt;For instance, what if i want to create/modify a partition for HW access?&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 13:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-API-included-in-Linux-Kernel-5-4-24/m-p/1271719#M173570</guid>
      <dc:creator>lorenzo_giraudi</dc:creator>
      <dc:date>2021-05-04T13:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW API included in Linux Kernel 5.4.24?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-API-included-in-Linux-Kernel-5-4-24/m-p/1272189#M173622</link>
      <description>&lt;P&gt;Hello lorenzo,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;They are already present, you can create a partition in hardware but not modifying these files since this file are just an api.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 13:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-API-included-in-Linux-Kernel-5-4-24/m-p/1272189#M173622</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-05-05T13:03:50Z</dc:date>
    </item>
  </channel>
</rss>