<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is there any documentation availabe for DIP swich configuration for the SABRE SDB board?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/230997#M17350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6 SDP / SDB design does not support the Serial Downloader mode directly.&lt;/P&gt;&lt;P&gt; According to section 4.1 (How to Enter Serial Download Mode for MFGTool)&lt;/P&gt;&lt;P&gt;of "i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"No dedicated boot dips are reserved for serial download mode on i.MX 6 SABRE-SD&lt;/P&gt;&lt;P&gt;boards. Therefore, a tricky method is used to enter serial download mode. For example,&lt;/P&gt;&lt;P&gt;set boot mode as SD3 boot (SW6 dip 2, 7 on others are off). Do not insert SD card into&lt;/P&gt;&lt;P&gt;SD3 slot, and power on the board. After "HID- Compliant device" is detected, it means&lt;/P&gt;&lt;P&gt;that the board has entered serial download mode. Insert the SD card into SD3 slot.&lt;/P&gt;&lt;P&gt;Another way to do this is to configure an invalid boot switch setting, for example, set all&lt;/P&gt;&lt;P&gt;the dips of SW6 to off."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Nov 2013 07:29:58 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-11-27T07:29:58Z</dc:date>
    <item>
      <title>How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is there any documentation availabe for DIP swich configuration for the SABRE SDB board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/230996#M17349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is there any documentation availabe for DIP swich configuration for the SABRE SDB board? I am able to load a image using the SD card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2013 07:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/230996#M17349</guid>
      <dc:creator>anandkumar</dc:creator>
      <dc:date>2013-11-27T07:02:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is there any documentation availabe for DIP swich configuration for the SABRE SDB board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/230997#M17350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6 SDP / SDB design does not support the Serial Downloader mode directly.&lt;/P&gt;&lt;P&gt; According to section 4.1 (How to Enter Serial Download Mode for MFGTool)&lt;/P&gt;&lt;P&gt;of "i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"No dedicated boot dips are reserved for serial download mode on i.MX 6 SABRE-SD&lt;/P&gt;&lt;P&gt;boards. Therefore, a tricky method is used to enter serial download mode. For example,&lt;/P&gt;&lt;P&gt;set boot mode as SD3 boot (SW6 dip 2, 7 on others are off). Do not insert SD card into&lt;/P&gt;&lt;P&gt;SD3 slot, and power on the board. After "HID- Compliant device" is detected, it means&lt;/P&gt;&lt;P&gt;that the board has entered serial download mode. Insert the SD card into SD3 slot.&lt;/P&gt;&lt;P&gt;Another way to do this is to configure an invalid boot switch setting, for example, set all&lt;/P&gt;&lt;P&gt;the dips of SW6 to off."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2013 07:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/230997#M17350</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-11-27T07:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is ther</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/1704609#M210773</link>
      <description>&lt;P&gt;Thank u for your response rapidly.That's useful.&lt;/P&gt;&lt;P&gt;Another question:&lt;/P&gt;&lt;P&gt;What need to do to the SD card first If I burn the SD card?For example, does it need to be formatted into a specific format, and does it require partitioning?&lt;/P&gt;&lt;P&gt;With the same question,What need I&amp;nbsp; do If I burn EMMC ?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Aug 2023 02:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/1704609#M210773</guid>
      <dc:creator>JunqiYu</dc:creator>
      <dc:date>2023-08-15T02:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is ther</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/1704651#M210783</link>
      <description>&lt;P&gt;Where can I find the file&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;"i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf"?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Aug 2023 03:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/1704651#M210783</guid>
      <dc:creator>JunqiYu</dc:creator>
      <dc:date>2023-08-15T03:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure the SW6 DIP switch to flash a program image on IMx6DQ SABRE SDB target? Is ther</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/1704850#M210798</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Where can I get the file&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;"i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" and related resources from NXP?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Aug 2023 07:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-the-SW6-DIP-switch-to-flash-a-program-image-on/m-p/1704850#M210798</guid>
      <dc:creator>JunqiYu</dc:creator>
      <dc:date>2023-08-15T07:58:49Z</dc:date>
    </item>
  </channel>
</rss>