<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: uBoot EMMC Size Support / IMX7</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271119#M173496</link>
    <description>&lt;P&gt;Hi Sean&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at similar issue on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/eMMC-8GB-to-4GB-crash-on-linux-yocto-boot/m-p/373231" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/eMMC-8GB-to-4GB-crash-on-linux-yocto-boot/m-p/373231&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Sun, 02 May 2021 22:55:25 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-05-02T22:55:25Z</dc:date>
    <item>
      <title>uBoot EMMC Size Support / IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271052#M173485</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have an existing custom image for my iMX7 board. The image works fine with 4GB / 8GB and 16GB EMMC. I have now received first units with 32GB EMMC but it does not boot uBoot.&lt;/P&gt;&lt;P&gt;If I do the same with the supplier's images, it would appear that the older images do not boot on the 32GB EMMC but work fine on the 4GB / 8GB and 16GB EMMC. The new supplier image boots on all size EMMC. Hence I believe that something might have changed in uBoot to work with high capacity EMMC.&lt;/P&gt;&lt;P&gt;Are you able to advise if this is the case please and what do I need to modify in my old image to make it work with 32GB EMMC please?&lt;/P&gt;&lt;P&gt;The older images report following version of uBoot:&amp;nbsp;&lt;/P&gt;&lt;TABLE width="656"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="656"&gt;U-Boot 2017.03 (Oct 02 2018 - 09:28:54 +0000)&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The newer images report:&lt;/P&gt;&lt;TABLE width="511"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="511"&gt;U-Boot 2018.03 (Jan 07 2021 - 02:39:24 -0600)&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can't seem to find any changes in the uBoot GIT repository that specifically reference EMMC size&amp;nbsp;&lt;SPAN&gt;changes.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have compared characteristic of 16GB and 32GB EMMC devices. Both support the same bus modes and speeds. Both support JEDEC 5.1. So I cannot see a difference there.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sat, 01 May 2021 06:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271052#M173485</guid>
      <dc:creator>Duracell</dc:creator>
      <dc:date>2021-05-01T06:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: uBoot EMMC Size Support / IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271119#M173496</link>
      <description>&lt;P&gt;Hi Sean&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at similar issue on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/eMMC-8GB-to-4GB-crash-on-linux-yocto-boot/m-p/373231" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/eMMC-8GB-to-4GB-crash-on-linux-yocto-boot/m-p/373231&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 02 May 2021 22:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271119#M173496</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-05-02T22:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: uBoot EMMC Size Support / IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271811#M173579</link>
      <description>&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;Thanks for you response.&lt;/P&gt;&lt;P&gt;I took a newer Ubuntu 20.0.4 image released and extracted the SPL (U-Boot SPL 2018.03) and injected this to replace our SPL (U-Boot SPL 2017.03) which now boots&amp;nbsp;U-Boot 2017.03 fine.&lt;/P&gt;&lt;P&gt;(1) Are you able to advise what changed between spl dated 2017.03 and 2018.03)?&lt;/P&gt;&lt;P&gt;(2) The start address of SPL is 0x400 (d'1024). What is the end address of SPL please? I have read that it is up to 8MB?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 16:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uBoot-EMMC-Size-Support-IMX7/m-p/1271811#M173579</guid>
      <dc:creator>Duracell</dc:creator>
      <dc:date>2021-05-04T16:05:14Z</dc:date>
    </item>
  </channel>
</rss>