<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 2GB RAM is used for Android 9 booting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270277#M173406</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have only&lt;STRONG&gt; 2GB RAM&lt;/STRONG&gt; in my &lt;STRONG&gt;IMX8QM Custom Board&lt;/STRONG&gt; (IMX8QM MEK have 6GB RAM).&lt;BR /&gt;But, my system image size is morethan 1GB. I want to know, is it enough for booting Android 9.&lt;/P&gt;&lt;P&gt;Memory configuration in&amp;nbsp;uboot,&lt;BR /&gt;&amp;nbsp; 1. sdram 1 size - 1GB&lt;BR /&gt;&amp;nbsp; 2. sdram 2 size - 1GB&lt;BR /&gt;&amp;nbsp; 3, Number of Banks - 8&lt;BR /&gt;&lt;BR /&gt;with this configuration I got iomap kernel hang.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I need some work around for 2GB RAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Apr 2021 10:23:01 GMT</pubDate>
    <dc:creator>vinothkumars</dc:creator>
    <dc:date>2021-04-29T10:23:01Z</dc:date>
    <item>
      <title>2GB RAM is used for Android 9 booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270277#M173406</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have only&lt;STRONG&gt; 2GB RAM&lt;/STRONG&gt; in my &lt;STRONG&gt;IMX8QM Custom Board&lt;/STRONG&gt; (IMX8QM MEK have 6GB RAM).&lt;BR /&gt;But, my system image size is morethan 1GB. I want to know, is it enough for booting Android 9.&lt;/P&gt;&lt;P&gt;Memory configuration in&amp;nbsp;uboot,&lt;BR /&gt;&amp;nbsp; 1. sdram 1 size - 1GB&lt;BR /&gt;&amp;nbsp; 2. sdram 2 size - 1GB&lt;BR /&gt;&amp;nbsp; 3, Number of Banks - 8&lt;BR /&gt;&lt;BR /&gt;with this configuration I got iomap kernel hang.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I need some work around for 2GB RAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 10:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270277#M173406</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2021-04-29T10:23:01Z</dc:date>
    </item>
    <item>
      <title>Re: 2GB RAM is used for Android 9 booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270592#M173427</link>
      <description>&lt;P&gt;I think you need to create very basic computer concept.&lt;/P&gt;
&lt;P&gt;The image size is not the size for the memory.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How many memory size needed depends on the use case. How many applications will be used.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The system image is rootfs. will not be entirely load to the memory.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It likes you have 2T hard disk for your x86/x64 compute and you have 32G memory.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;and your concept is if I want to use this 2T disk computer, I need 2T memory as well.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 01:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270592#M173427</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2021-04-30T01:18:08Z</dc:date>
    </item>
    <item>
      <title>Re: 2GB RAM is used for Android 9 booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270863#M173469</link>
      <description>&lt;P&gt;Good&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 13:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2GB-RAM-is-used-for-Android-9-booting/m-p/1270863#M173469</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-04-30T13:20:50Z</dc:date>
    </item>
  </channel>
</rss>