<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8M HDR10 Intro &amp;amp; Application Support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1269277#M173322</link>
    <description>&lt;P&gt;&lt;SPAN&gt;1. if it is possible for MIPI-CSI camera input to be diverted into the i.MX8M HDR10 processor for output&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;Yes,8mp support(only 8mp has isp)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2.HDR support:&lt;BR /&gt;— HDR10 with 2084 and 2020 color spaces&lt;BR /&gt;— Dolby Vision single and dual layer formats&lt;BR /&gt;— HLG&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3.ISP&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The ISP is connected to a MIPI-CSI interface and receives 1 pixel/clock from the CSI Rx&lt;BR /&gt;Controller. Key features of the ISP include:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;• Input Formats:&lt;BR /&gt;• YCbCr420&lt;BR /&gt;• YCbCr422&lt;BR /&gt;• RAW8&lt;BR /&gt;• RAW10&lt;BR /&gt;• RAW12&lt;BR /&gt;• RAW14&lt;BR /&gt;• Wide Dynamic Range (local tone mapping)&lt;BR /&gt;• High Dynamic Range (HDR)&lt;BR /&gt;• Native HDR sensor with compand output and max 14-bit compressed input&lt;BR /&gt;• 2-exposure and 3-exposure line-interleaved (staggered) HDR&lt;BR /&gt;• Full resolution for multiple exposures is output by the image sensor, and the&lt;BR /&gt;sensor outputs are interleaved on a per-line basis. No impact to vertical&lt;BR /&gt;resolution, but frame rate is reduced by a factor of 2 (for 2-exposure HDR)&lt;BR /&gt;or 3 (for 3-exposure HDR).&lt;BR /&gt;• Referred to as DOL-HDR (Digital Overlap High Dynamic Range) and as&lt;BR /&gt;Staggered HDR (12-bit x3)&lt;BR /&gt;• A separate Dewarp engine is also supported to adjust an image (i.e. fisheye lens) at a&lt;BR /&gt;resolution up to the max resolution supported by the ISP.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 28 Apr 2021 03:26:21 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2021-04-28T03:26:21Z</dc:date>
    <item>
      <title>i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255425#M171913</link>
      <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;My team and I are interested in knowing more info on the actual application / how-to for HDR10 implementation on i.MX8M.&lt;/P&gt;&lt;P&gt;Internet searches tend to only provide general idea of HDR10. 10 bits color depth, meta data which allows additional brightness info and gamma curve...etc.&amp;nbsp;but does not provide much details on how HDR is achieved and what is needed for both HW &amp;amp; SW.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the HDR10 processor for i.MX8M a plug-in and go solution? Being HW wise I can simply connect HDR10 source (WiFi streaming Netflix or HDR10 camera input form MIPI-CSI) and eDP LCD that supports HDR10?&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 02:48:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255425#M171913</guid>
      <dc:creator>howard_kuo97</dc:creator>
      <dc:date>2021-04-01T02:48:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255457#M171914</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;We realize the HDR10 and Dolby Vision in i.MX8MD/i.MX8MQ HW and software,you can use&amp;nbsp;&lt;SPAN&gt;WiFi streaming Netflix to play HDR video.But the HDR camera needs driver porting.Display component is completed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Zhiming&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 03:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255457#M171914</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-04-01T03:24:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255470#M171916</link>
      <description>&lt;P&gt;Hi Zhiming:&lt;BR /&gt;&lt;BR /&gt;Thank you for the prompt response. For software is it ready for Linux? and is there a suggested testing method?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Howard Kuo&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 03:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255470#M171916</guid>
      <dc:creator>howard_kuo97</dc:creator>
      <dc:date>2021-04-01T03:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255480#M171917</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;i.MX8MP is most powerful evk now, it supports HDR camera capture and HDR display.&lt;/P&gt;
&lt;P&gt;Tests:&lt;A href="https://imxdev.gitlab.io/tutorial/How_to_use_dual_display_on_i.MX8_including_4k_decoding/" target="_blank"&gt;https://imxdev.gitlab.io/tutorial/How_to_use_dual_display_on_i.MX8_including_4k_decoding/&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I don't recommand&amp;nbsp; i.MX8MQ personally.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 04:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1255480#M171917</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-04-01T04:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1268577#M173250</link>
      <description>&lt;P&gt;Hi Zhiming &amp;amp; NXP Team:&lt;/P&gt;&lt;P&gt;Upon further evaluation, for our application we would like to know if it is possible for MIPI-CSI camera input to be diverted into the i.MX8M HDR10 processor for output? Besides for the camera driver porting, it looks like i.MX8M only support BT2020 / ST2084 format? So we are wondering if there are other missing links or a need for additional ISP? We would like to know if it is even feasible.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 06:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1268577#M173250</guid>
      <dc:creator>howard_kuo97</dc:creator>
      <dc:date>2021-04-27T06:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1269277#M173322</link>
      <description>&lt;P&gt;&lt;SPAN&gt;1. if it is possible for MIPI-CSI camera input to be diverted into the i.MX8M HDR10 processor for output&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;Yes,8mp support(only 8mp has isp)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2.HDR support:&lt;BR /&gt;— HDR10 with 2084 and 2020 color spaces&lt;BR /&gt;— Dolby Vision single and dual layer formats&lt;BR /&gt;— HLG&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3.ISP&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The ISP is connected to a MIPI-CSI interface and receives 1 pixel/clock from the CSI Rx&lt;BR /&gt;Controller. Key features of the ISP include:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;• Input Formats:&lt;BR /&gt;• YCbCr420&lt;BR /&gt;• YCbCr422&lt;BR /&gt;• RAW8&lt;BR /&gt;• RAW10&lt;BR /&gt;• RAW12&lt;BR /&gt;• RAW14&lt;BR /&gt;• Wide Dynamic Range (local tone mapping)&lt;BR /&gt;• High Dynamic Range (HDR)&lt;BR /&gt;• Native HDR sensor with compand output and max 14-bit compressed input&lt;BR /&gt;• 2-exposure and 3-exposure line-interleaved (staggered) HDR&lt;BR /&gt;• Full resolution for multiple exposures is output by the image sensor, and the&lt;BR /&gt;sensor outputs are interleaved on a per-line basis. No impact to vertical&lt;BR /&gt;resolution, but frame rate is reduced by a factor of 2 (for 2-exposure HDR)&lt;BR /&gt;or 3 (for 3-exposure HDR).&lt;BR /&gt;• Referred to as DOL-HDR (Digital Overlap High Dynamic Range) and as&lt;BR /&gt;Staggered HDR (12-bit x3)&lt;BR /&gt;• A separate Dewarp engine is also supported to adjust an image (i.e. fisheye lens) at a&lt;BR /&gt;resolution up to the max resolution supported by the ISP.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 03:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/1269277#M173322</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-04-28T03:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M HDR10 Intro &amp; Application Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/2108349#M237806</link>
      <description>&lt;P&gt;Is there any particular reason for mentioning "I don't recommand&amp;nbsp; i.MX8MQ personally." in your reply?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using NXP BSP6.6.52 image on IMX8MQ-EVK-DP version and HDR videos don't look HDR on the panel, it appears to play in SDR mode, we are using waylandsink.&lt;/P&gt;&lt;P&gt;We confirmed that our panel supports HDR10 in BT2020_RGB mode.&lt;/P&gt;</description>
      <pubDate>Sat, 31 May 2025 20:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-HDR10-Intro-amp-Application-Support/m-p/2108349#M237806</guid>
      <dc:creator>gkasimandiri</dc:creator>
      <dc:date>2025-05-31T20:22:54Z</dc:date>
    </item>
  </channel>
</rss>