<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: u-boot DDR size in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268867#M173280</link>
    <description>&lt;P&gt;Thanks,&amp;nbsp;it did the trick.&lt;/P&gt;&lt;P&gt;I do not need really the op-tee so I am good.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 27 Apr 2021 12:06:13 GMT</pubDate>
    <dc:creator>Giacomo_</dc:creator>
    <dc:date>2021-04-27T12:06:13Z</dc:date>
    <item>
      <title>u-boot DDR size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268147#M173210</link>
      <description>&lt;P&gt;Hello support team,&lt;BR /&gt;we have developed a proprietary board derived from the NXP evaboard imx8mqevk.&lt;BR /&gt;The DDR memory format has changed to 2GB but u-boot always states 3GB of memory (the same size of the evaboard).&lt;/P&gt;&lt;P&gt;Yocto version is Zeus (imx-5.4.24-2.1.0)&lt;/P&gt;&lt;P&gt;The boot output:&lt;BR /&gt;&lt;EM&gt;------------------------------------------------------------------------------------------&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;U-Boot 2020.04-5.4.24-2.1.0+g4979a99482 (Apr 26 2021 - 10:03:28 +0000)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CPU: i.MX8MD rev2.1 1500 MHz (running at 1000 MHz)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: Commercial temperature grade (0C to 95C) at 42C&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset cause: POR&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Model: NXP i.MX8MQ EVK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 3 GiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x50]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;lt;snip&amp;gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;------------------------------------------------------------------------------------------&lt;/EM&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;We replaced the file generated by the mscale_ddr_tool (nightly test passed) in file: "board/freescale/imx8mq_evk/lpddr4_timing.c"&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;LI&gt;Fixed the memory node in device tree: "arch/arm/dts/imx8mq-evk.dts"&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;EM&gt;memory@40000000 {&lt;BR /&gt;&lt;/EM&gt;&lt;EM&gt;&amp;nbsp; &amp;nbsp; device_type = "memory";&lt;BR /&gt;&lt;/EM&gt;&lt;EM&gt;&amp;nbsp; &amp;nbsp; reg = &amp;lt;0x00000000 0x40000000 0 0x80000000&amp;gt;;&lt;BR /&gt;&lt;/EM&gt;&lt;EM&gt;};&lt;BR /&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;Changed the constant PHYS_SDRAM_SIZE in file: "include/configs/imx8mq_evk.h"&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Still no luck, what else are we&amp;nbsp;&lt;SPAN&gt;missing?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 12:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268147#M173210</guid>
      <dc:creator>Giacomo_</dc:creator>
      <dc:date>2021-04-26T12:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot DDR size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268393#M173229</link>
      <description>&lt;P&gt;Hi Giacomo&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;just for test one can try to build without OPTee, as described in sect.5.6.10 OP-TEE enablement&lt;/P&gt;
&lt;P&gt;Yocto Guide included in&amp;nbsp; &lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_LINUX_DOCS" target="_blank" rel="noopener"&gt;Documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also i.MX8M Mini EVK has 2GB configuration and one can look at its configs for comparison.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 00:28:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268393#M173229</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-04-27T00:28:10Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot DDR size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268867#M173280</link>
      <description>&lt;P&gt;Thanks,&amp;nbsp;it did the trick.&lt;/P&gt;&lt;P&gt;I do not need really the op-tee so I am good.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 12:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/1268867#M173280</guid>
      <dc:creator>Giacomo_</dc:creator>
      <dc:date>2021-04-27T12:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot DDR size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/2092934#M237005</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please see my same issue, actually never fixed , thank you every much for you help. it seems nobody use&amp;nbsp; optee on maaxboard or imx8mq_evk from yocto zeus.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/after-enabling-optee-in-maaxboard-memory-size-change-from-2G-to/m-p/2075204#M235978" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/after-enabling-optee-in-maaxboard-memory-size-change-from-2G-to/m-p/2075204#M235978&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 May 2025 16:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-DDR-size/m-p/2092934#M237005</guid>
      <dc:creator>gonewithwind-peter</dc:creator>
      <dc:date>2025-05-07T16:10:41Z</dc:date>
    </item>
  </channel>
</rss>