<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX8M Mini eCSPI boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-eCSPI-boot/m-p/1267899#M173177</link>
    <description>&lt;P&gt;On a system of ours, we have successfully implemented the eCSPI boot for the iMX8M Nano.&lt;/P&gt;&lt;P&gt;When using the same approach for the iMX8M Mini, I have the following question.&lt;BR /&gt;So far we have been able to start the SPL from eCSPI, but after that I'm not sure how the SPL is expected to load the rest of the bootloader (U-Boot) from flash.&lt;/P&gt;&lt;P&gt;The Nano uses the BootROM API for this, but looking at the U-Boot code this API is not implemented for the Mini. Is it a possibility to use the BootROM API on the Mini for purpose of eCSPI boot?&lt;/P&gt;&lt;P&gt;The Mini uses AHB access to load data via FlexSPI/QSPI, but I'm not sure this access method can be used for the eCSPI1 interface. Is this possible?&lt;/P&gt;</description>
    <pubDate>Mon, 26 Apr 2021 07:02:44 GMT</pubDate>
    <dc:creator>wouher</dc:creator>
    <dc:date>2021-04-26T07:02:44Z</dc:date>
    <item>
      <title>iMX8M Mini eCSPI boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-eCSPI-boot/m-p/1267899#M173177</link>
      <description>&lt;P&gt;On a system of ours, we have successfully implemented the eCSPI boot for the iMX8M Nano.&lt;/P&gt;&lt;P&gt;When using the same approach for the iMX8M Mini, I have the following question.&lt;BR /&gt;So far we have been able to start the SPL from eCSPI, but after that I'm not sure how the SPL is expected to load the rest of the bootloader (U-Boot) from flash.&lt;/P&gt;&lt;P&gt;The Nano uses the BootROM API for this, but looking at the U-Boot code this API is not implemented for the Mini. Is it a possibility to use the BootROM API on the Mini for purpose of eCSPI boot?&lt;/P&gt;&lt;P&gt;The Mini uses AHB access to load data via FlexSPI/QSPI, but I'm not sure this access method can be used for the eCSPI1 interface. Is this possible?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 07:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-eCSPI-boot/m-p/1267899#M173177</guid>
      <dc:creator>wouher</dc:creator>
      <dc:date>2021-04-26T07:02:44Z</dc:date>
    </item>
  </channel>
</rss>