<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6ULL DRR CALIBRATION FAILED</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-DRR-CALIBRATION-FAILED/m-p/1266602#M173056</link>
    <description>&lt;P&gt;I used ddr_stress_tester to test my pacba, but failed at calibration.&lt;/P&gt;&lt;P&gt;Then,I Set Voltage to 1.75, it tests success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q1: How do I set voltage to source code?Because&amp;nbsp; when brushing machine is also failed .so it can not go to the linux system. should I modify DCD data of code on uboot?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q2: for his failed of calibration,&amp;nbsp;What might be the cause? how&amp;nbsp; will we modifiy PCB?&lt;/P&gt;</description>
    <pubDate>Thu, 22 Apr 2021 10:55:13 GMT</pubDate>
    <dc:creator>Oman</dc:creator>
    <dc:date>2021-04-22T10:55:13Z</dc:date>
    <item>
      <title>IMX6ULL DRR CALIBRATION FAILED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-DRR-CALIBRATION-FAILED/m-p/1266602#M173056</link>
      <description>&lt;P&gt;I used ddr_stress_tester to test my pacba, but failed at calibration.&lt;/P&gt;&lt;P&gt;Then,I Set Voltage to 1.75, it tests success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q1: How do I set voltage to source code?Because&amp;nbsp; when brushing machine is also failed .so it can not go to the linux system. should I modify DCD data of code on uboot?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q2: for his failed of calibration,&amp;nbsp;What might be the cause? how&amp;nbsp; will we modifiy PCB?&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 10:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-DRR-CALIBRATION-FAILED/m-p/1266602#M173056</guid>
      <dc:creator>Oman</dc:creator>
      <dc:date>2021-04-22T10:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULL DRR CALIBRATION FAILED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-DRR-CALIBRATION-FAILED/m-p/1266934#M173082</link>
      <description>&lt;P&gt;Hi Barry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. one can add codes to dcd header or increase voltage in uboot board file&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6sabresd/mx6sabresd.c?h=imx_v2020.04_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6sabresd/mx6sabresd.c?h=imx_v2020.04_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2. calibration may fail due to power supplies voltages, one can check power requirements,&lt;/P&gt;
&lt;P&gt;like ripplies in&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 23 Apr 2021 00:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-DRR-CALIBRATION-FAILED/m-p/1266934#M173082</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-04-23T00:48:23Z</dc:date>
    </item>
  </channel>
</rss>