<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: I.MX8DXP board bring up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8DXP-board-bring-up/m-p/1265041#M172913</link>
    <description>&lt;P&gt;1\ You need to use the qx&lt;/P&gt;
&lt;P&gt;2\No, you do not need. There are different machine name imx8qxpc0mek imx8dxmek, and uboot configue they are uboot_config_imx8dxmek&amp;nbsp;uboot_config_imx8qxpc0mek&lt;/P&gt;
&lt;P&gt;3\ No, But they use different&amp;nbsp; device tree, On i.MX 8QuadMax and 8QuadXPlus, multiple partitions are supported.&lt;BR /&gt;Due to the board design, flash.bin and the DTB need to be matched. If&lt;BR /&gt;flash.bin includes the Cortex-M4 partition, use x-rpmsg.dtb.&lt;/P&gt;</description>
    <pubDate>Tue, 20 Apr 2021 09:36:35 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2021-04-20T09:36:35Z</dc:date>
    <item>
      <title>I.MX8DXP board bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8DXP-board-bring-up/m-p/1233242#M169700</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on BSP L4.14.98_2.3.3, I have some questions about porting i.MX8DXP SOC.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;scfw (v1.3.3) porting kit: no die target in makefile for DXP, only qm/qx/dxl supported. how to build to suit DXP SOC, or just use "&lt;EM&gt;&lt;STRONG&gt;qx" &lt;/STRONG&gt;&lt;/EM&gt;for DXP as same as QXP?&lt;/LI&gt;&lt;LI&gt;linux/u-boot: no machine or configuration for DXP, do I need porting this by myself(reference from imx8qxpc0mek)? or any better suggestion?&lt;/LI&gt;&lt;LI&gt;MCUXpresso SDK(for CM4): if the part number of DXP is MiMX8DX6AVLFZAC, almost pin-to-pin compatible as MiMX8QX6AVLFZAC(imx8qxpc0mek used), do I need MUST to change this SDK necessarily?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 03:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8DXP-board-bring-up/m-p/1233242#M169700</guid>
      <dc:creator>yellow_huang</dc:creator>
      <dc:date>2021-02-19T03:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8DXP board bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8DXP-board-bring-up/m-p/1265041#M172913</link>
      <description>&lt;P&gt;1\ You need to use the qx&lt;/P&gt;
&lt;P&gt;2\No, you do not need. There are different machine name imx8qxpc0mek imx8dxmek, and uboot configue they are uboot_config_imx8dxmek&amp;nbsp;uboot_config_imx8qxpc0mek&lt;/P&gt;
&lt;P&gt;3\ No, But they use different&amp;nbsp; device tree, On i.MX 8QuadMax and 8QuadXPlus, multiple partitions are supported.&lt;BR /&gt;Due to the board design, flash.bin and the DTB need to be matched. If&lt;BR /&gt;flash.bin includes the Cortex-M4 partition, use x-rpmsg.dtb.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 09:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8DXP-board-bring-up/m-p/1265041#M172913</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-04-20T09:36:35Z</dc:date>
    </item>
  </channel>
</rss>