<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using Internal oscillator for RTC_XTAL in i.MX6 Solo in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265014#M172910</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are planning to use internal oscillator instead of connecting external crystal to the RTC_XTAL inputs of iMX6 solo. For enabling internal oscillator, we have connected RTC_XTALI pin to ground and left the RTC_XTALO unconnected.&amp;nbsp; Can you let me know if any function in i.MX6 can be affected when the i.MX6 is active because of the poor accuracy of the internal oscillator?&lt;/P&gt;&lt;P&gt;Note, We are not planning on using the RTC in our board. The i.MX6 will always be active in our board and no suspend or power down mode implementation is required.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sivaraj&lt;/P&gt;</description>
    <pubDate>Tue, 20 Apr 2021 09:15:01 GMT</pubDate>
    <dc:creator>sivaraj</dc:creator>
    <dc:date>2021-04-20T09:15:01Z</dc:date>
    <item>
      <title>Using Internal oscillator for RTC_XTAL in i.MX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265014#M172910</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are planning to use internal oscillator instead of connecting external crystal to the RTC_XTAL inputs of iMX6 solo. For enabling internal oscillator, we have connected RTC_XTALI pin to ground and left the RTC_XTALO unconnected.&amp;nbsp; Can you let me know if any function in i.MX6 can be affected when the i.MX6 is active because of the poor accuracy of the internal oscillator?&lt;/P&gt;&lt;P&gt;Note, We are not planning on using the RTC in our board. The i.MX6 will always be active in our board and no suspend or power down mode implementation is required.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sivaraj&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 09:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265014#M172910</guid>
      <dc:creator>sivaraj</dc:creator>
      <dc:date>2021-04-20T09:15:01Z</dc:date>
    </item>
    <item>
      <title>Re: Using Internal oscillator for RTC_XTAL in i.MX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265072#M172917</link>
      <description>&lt;P&gt;Hi Sivaraj&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for possible issues one can look at ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy..&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;Chip Errata for the i.MX 6Solo/6DualLite&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 10:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265072#M172917</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-04-20T10:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: Using Internal oscillator for RTC_XTAL in i.MX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265090#M172924</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;We are using i.MX6 processor with silicon revision 1.3 only.&lt;/P&gt;&lt;P&gt;Can you please confirm if there will not be any issues in this due to the internal oscillator accuracy in this Silicon Revision 1.3 and future revisions?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sivaraj&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 10:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265090#M172924</guid>
      <dc:creator>sivaraj</dc:creator>
      <dc:date>2021-04-20T10:54:56Z</dc:date>
    </item>
    <item>
      <title>Re: Using Internal oscillator for RTC_XTAL in i.MX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265155#M172929</link>
      <description>&lt;P&gt;yes boot issue is fixed for rev.1.3, however if it is used as clock source for gpt, wdog or other&lt;/P&gt;
&lt;P&gt;module it is necessary to consider that it may be up to two times faster than a 32 kHz external crystal oscillator.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 12:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Internal-oscillator-for-RTC-XTAL-in-i-MX6-Solo/m-p/1265155#M172929</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-04-20T12:56:35Z</dc:date>
    </item>
  </channel>
</rss>