<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8M yocto linux NTP bug (aka Y2K38)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1265000#M172906</link>
    <description>&lt;P&gt;The solution is to use the latest yocto version: "Dunfell".&lt;/P&gt;&lt;P&gt;In that version the bug has been fixed.&lt;/P&gt;</description>
    <pubDate>Tue, 20 Apr 2021 09:03:53 GMT</pubDate>
    <dc:creator>agmc1971</dc:creator>
    <dc:date>2021-04-20T09:03:53Z</dc:date>
    <item>
      <title>IMX8M yocto linux NTP bug (aka Y2K38)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1264476#M172836</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;my IMx8M yocto (SUMO) linux microcontroller evidence a problem in setting date/hour using NTP service if the system clock (RTC) have a date beyhond the 2038. If I write the year that is less than that date , NTP succeed to setting the right date/time.&lt;/P&gt;&lt;P&gt;Do you experienced similar issue, and if yes, what is the solution to this bug?&lt;/P&gt;&lt;P&gt;Thanks in advance for your help!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;AG&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 15:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1264476#M172836</guid>
      <dc:creator>agmc1971</dc:creator>
      <dc:date>2021-04-19T15:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M yocto linux NTP bug (aka Y2K38)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1265000#M172906</link>
      <description>&lt;P&gt;The solution is to use the latest yocto version: "Dunfell".&lt;/P&gt;&lt;P&gt;In that version the bug has been fixed.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 09:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1265000#M172906</guid>
      <dc:creator>agmc1971</dc:creator>
      <dc:date>2021-04-20T09:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M yocto linux NTP bug (aka Y2K38)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1266426#M173037</link>
      <description>&lt;P&gt;Actually Linux starting with version 5.6 has 64-bit time_t (the type is used for the time) even on 32-bit architectures.&lt;BR /&gt;Now I see dates after the year 2038 are supported:&lt;/P&gt;
&lt;P&gt;root@imx8mqevk:~# date 050113132222&lt;BR /&gt;Wed May 1 13:13:00 UTC 2222&lt;BR /&gt;root@imx8mqevk:~# date +%s &lt;BR /&gt;7962757988&lt;BR /&gt;root@imx8mqevk:~# touch file&lt;BR /&gt;root@imx8mqevk:~# ls -l --time-style=+%s file&lt;BR /&gt;0 -rw-r--r-- 1 root root 0 7962757992 file&lt;BR /&gt;root@imx8mqevk:~#&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 07:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-yocto-linux-NTP-bug-aka-Y2K38/m-p/1266426#M173037</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-04-22T07:32:20Z</dc:date>
    </item>
  </channel>
</rss>