<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6 secure boot - upgrade u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1263975#M172781</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;But my question is still open and not answered.&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;rsm4&lt;/P&gt;</description>
    <pubDate>Mon, 19 Apr 2021 04:09:40 GMT</pubDate>
    <dc:creator>rsm4</dc:creator>
    <dc:date>2021-04-19T04:09:40Z</dc:date>
    <item>
      <title>imx6 secure boot - upgrade u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1258880#M172260</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a secure boot on imx6. The u-boot is located at QSPI flash. How is it possible to upgrade/update the u-boot. It must be mentioned that it shall be updated before a SW other than u-boot is executed. Also SPL is NOT used. Is there still a way to tell BOOT_ROM to boot from a different media (e.g.: eMMC) other than QSPI? Also no possibility given to modify the boot mode!&lt;BR /&gt;&lt;BR /&gt;Following fuses are used:&lt;BR /&gt;BT_DIR_DIS = "1" --&amp;gt;&amp;nbsp;Necessary for secure boot according RM&lt;BR /&gt;BT_FUSE_SEL = "1" --&amp;gt; Use Fuses instead GPIO&lt;BR /&gt;SEC_CONFIG [1:0] = "0x10" --&amp;gt; Closed&lt;BR /&gt;BOOT_CFG1[7:0] = "0x10" --&amp;gt; QSPI Boot&lt;/P&gt;&lt;P&gt;It would be fine to get an answer on this!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;rsm4&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 12:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1258880#M172260</guid>
      <dc:creator>rsm4</dc:creator>
      <dc:date>2021-04-08T12:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 secure boot - upgrade u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1263025#M172672</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may find it helpful to refer to the following document for secure boot:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN4581" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=AN4581&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;or:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12056.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12056.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Ivan.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 18:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1263025#M172672</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2021-04-15T18:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 secure boot - upgrade u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1263975#M172781</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;But my question is still open and not answered.&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;rsm4&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 04:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-secure-boot-upgrade-u-boot/m-p/1263975#M172781</guid>
      <dc:creator>rsm4</dc:creator>
      <dc:date>2021-04-19T04:09:40Z</dc:date>
    </item>
  </channel>
</rss>