<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is iMX 6 SoloX with two WiFi module working simultaneously? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1261218#M172513</link>
    <description>Hello, I am going to apply two WiFi module to i.MX 6 SoloX SD2 and SD3. One WiFi module is connected to SD2 as Input and the other is connected to SD3 as Output. I wonder if SDK of i.MX 6 SoloX supports the operating of two WiFi module at the same time. Thanks, Andy</description>
    <pubDate>Tue, 13 Apr 2021 10:49:29 GMT</pubDate>
    <dc:creator>andy_kim</dc:creator>
    <dc:date>2021-04-13T10:49:29Z</dc:date>
    <item>
      <title>Is iMX 6 SoloX with two WiFi module working simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1261218#M172513</link>
      <description>Hello, I am going to apply two WiFi module to i.MX 6 SoloX SD2 and SD3. One WiFi module is connected to SD2 as Input and the other is connected to SD3 as Output. I wonder if SDK of i.MX 6 SoloX supports the operating of two WiFi module at the same time. Thanks, Andy</description>
      <pubDate>Tue, 13 Apr 2021 10:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1261218#M172513</guid>
      <dc:creator>andy_kim</dc:creator>
      <dc:date>2021-04-13T10:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: Is iMX 6 SoloX with two WiFi module working simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1270284#M173407</link>
      <description>&lt;P&gt;There seems to be no experience of connecting two WiFi modules to a single i.MX6 &lt;BR /&gt;series processor. However, there should be no problem from the hardware point &lt;BR /&gt;of view if correctly configuring a driver instance bindings.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 10:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1270284#M173407</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-04-29T10:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: Is iMX 6 SoloX with two WiFi module working simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1270685#M173437</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your confirmation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 06:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-iMX-6-SoloX-with-two-WiFi-module-working-simultaneously/m-p/1270685#M173437</guid>
      <dc:creator>andy_kim</dc:creator>
      <dc:date>2021-04-30T06:35:29Z</dc:date>
    </item>
  </channel>
</rss>