<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx8 optee enanched OpenSSL example in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-optee-enanched-OpenSSL-example/m-p/1260622#M172455</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm interested to working with the Enhanced OpenSSL example (AN12632)&lt;BR /&gt;but with the iMX8 architecture.&lt;/P&gt;&lt;P&gt;When I try to compile optee-os with CFG_IMXCRYPT enabled, I give an error and then I see that this define is disabled by design when use it on iMX8&lt;/P&gt;&lt;P&gt;Is possible to use this example or any other similar (openssl+optee) with iMX8?&lt;/P&gt;</description>
    <pubDate>Mon, 12 Apr 2021 14:25:26 GMT</pubDate>
    <dc:creator>matteo-facchinetti</dc:creator>
    <dc:date>2021-04-12T14:25:26Z</dc:date>
    <item>
      <title>imx8 optee enanched OpenSSL example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-optee-enanched-OpenSSL-example/m-p/1260622#M172455</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm interested to working with the Enhanced OpenSSL example (AN12632)&lt;BR /&gt;but with the iMX8 architecture.&lt;/P&gt;&lt;P&gt;When I try to compile optee-os with CFG_IMXCRYPT enabled, I give an error and then I see that this define is disabled by design when use it on iMX8&lt;/P&gt;&lt;P&gt;Is possible to use this example or any other similar (openssl+optee) with iMX8?&lt;/P&gt;</description>
      <pubDate>Mon, 12 Apr 2021 14:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-optee-enanched-OpenSSL-example/m-p/1260622#M172455</guid>
      <dc:creator>matteo-facchinetti</dc:creator>
      <dc:date>2021-04-12T14:25:26Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 optee enanched OpenSSL example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-optee-enanched-OpenSSL-example/m-p/1273282#M173696</link>
      <description>&lt;P&gt;Hi&amp;nbsp;matteo-facchinett,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the moment there is no example as the optee is not supported on the imx8 devices.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for that.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Thu, 06 May 2021 23:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-optee-enanched-OpenSSL-example/m-p/1273282#M173696</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-05-06T23:12:38Z</dc:date>
    </item>
  </channel>
</rss>