<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6Q SDCard Boot configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDCard-Boot-configuration/m-p/1259836#M172371</link>
    <description>&lt;P&gt;Could someone explain the meaning of&amp;nbsp;BOOT_CFG1[4] (0=normal and 1=fastboot)? When use one or another? and the practice diference running a Linux or Android OS from SDCard with one option or another configured.&lt;/P&gt;</description>
    <pubDate>Fri, 09 Apr 2021 18:13:01 GMT</pubDate>
    <dc:creator>leonardoprates</dc:creator>
    <dc:date>2021-04-09T18:13:01Z</dc:date>
    <item>
      <title>IMX6Q SDCard Boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDCard-Boot-configuration/m-p/1259836#M172371</link>
      <description>&lt;P&gt;Could someone explain the meaning of&amp;nbsp;BOOT_CFG1[4] (0=normal and 1=fastboot)? When use one or another? and the practice diference running a Linux or Android OS from SDCard with one option or another configured.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 18:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDCard-Boot-configuration/m-p/1259836#M172371</guid>
      <dc:creator>leonardoprates</dc:creator>
      <dc:date>2021-04-09T18:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q SDCard Boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDCard-Boot-configuration/m-p/1260949#M172482</link>
      <description>&lt;P&gt;Hi leonardoprates,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Well usually the main difference is the speed of the boot-up During the card initialization, the ROM boot code attempts to set the boot partition for all&lt;BR /&gt;SD, eSD, and SDXC devices. If this fails, the boot code assumes that the card is a normal&lt;BR /&gt;SD or SDXC card. If it does not fail, the boot code assumes it is an eSD card. After the&lt;BR /&gt;initialization phase is over, the boot code switches to a higher frequency (25 MHz in the&lt;BR /&gt;normal-speed mode or 50 MHz in the high-speed mode).&lt;/P&gt;
&lt;P&gt;Fastboot is a protocol used to update the flash filesystem in Android devices from a host over USB. It allows the flashing of unsigned partition images.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps you.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 04:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDCard-Boot-configuration/m-p/1260949#M172482</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-04-13T04:29:33Z</dc:date>
    </item>
  </channel>
</rss>