<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.Mx 8M Nano - Cortex M7 Core frequency Selection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx-8M-Nano-Cortex-M7-Core-frequency-Selection/m-p/1259822#M172369</link>
    <description>&lt;P&gt;Good Morning,&lt;/P&gt;&lt;P&gt;As I understand Cortex M7 Core frequency can be configures to 600Mhz or 750Mhz.&lt;/P&gt;&lt;P&gt;Looking at datasheet, the only reference for this configuration is the Voltage Value (0.85 for 600Mhz and 0.95 for 750Mhz)&lt;/P&gt;&lt;P&gt;At my case, I will use 0.85V for 600Mhz.&lt;/P&gt;&lt;P&gt;My question is, how do I configure the internal multipliers of M7 to run at this frequency ? Or I just need to power it with 0.85V and the frequency is consequence.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sergio Spader&lt;/P&gt;</description>
    <pubDate>Fri, 09 Apr 2021 17:33:47 GMT</pubDate>
    <dc:creator>sergiospader</dc:creator>
    <dc:date>2021-04-09T17:33:47Z</dc:date>
    <item>
      <title>i.Mx 8M Nano - Cortex M7 Core frequency Selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx-8M-Nano-Cortex-M7-Core-frequency-Selection/m-p/1259822#M172369</link>
      <description>&lt;P&gt;Good Morning,&lt;/P&gt;&lt;P&gt;As I understand Cortex M7 Core frequency can be configures to 600Mhz or 750Mhz.&lt;/P&gt;&lt;P&gt;Looking at datasheet, the only reference for this configuration is the Voltage Value (0.85 for 600Mhz and 0.95 for 750Mhz)&lt;/P&gt;&lt;P&gt;At my case, I will use 0.85V for 600Mhz.&lt;/P&gt;&lt;P&gt;My question is, how do I configure the internal multipliers of M7 to run at this frequency ? Or I just need to power it with 0.85V and the frequency is consequence.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sergio Spader&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 17:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx-8M-Nano-Cortex-M7-Core-frequency-Selection/m-p/1259822#M172369</guid>
      <dc:creator>sergiospader</dc:creator>
      <dc:date>2021-04-09T17:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx 8M Nano - Cortex M7 Core frequency Selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx-8M-Nano-Cortex-M7-Core-frequency-Selection/m-p/1259939#M172376</link>
      <description>&lt;P&gt;Hi Sergio&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for configuring M7 frequency one can look at Table 5-1. Clock Root Table (ARM_M7_CLK_ROOT),&lt;/P&gt;
&lt;P&gt;Figure 5-2. CCM input clock sources, sect.5.1.8.25 M7 Alternate PLL General Function Control Register&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX8MNRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Nano Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In general it is not changed automatically with voltage change.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 10 Apr 2021 00:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx-8M-Nano-Cortex-M7-Core-frequency-Selection/m-p/1259939#M172376</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-04-10T00:42:22Z</dc:date>
    </item>
  </channel>
</rss>