<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8QM Power consumption</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Power-consumption/m-p/1259813#M172368</link>
    <description>Hi all, for our integration specification we need some information about the power consumption of the IMX8QM building block. For now we don't need a very detailed description but a rough approximation in order to dimension the power supply for the host system. We plan to supply the PMICs only with a single +5V power supply rail.&amp;nbsp; The parameters we need are following: 1) Maximum power consumption 2) Peak current&amp;nbsp; 3) Rise time for the +5V input rail during start up BR Gery</description>
    <pubDate>Fri, 09 Apr 2021 17:01:54 GMT</pubDate>
    <dc:creator>gerassimos_pari</dc:creator>
    <dc:date>2021-04-09T17:01:54Z</dc:date>
    <item>
      <title>IMX8QM Power consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Power-consumption/m-p/1259813#M172368</link>
      <description>Hi all, for our integration specification we need some information about the power consumption of the IMX8QM building block. For now we don't need a very detailed description but a rough approximation in order to dimension the power supply for the host system. We plan to supply the PMICs only with a single +5V power supply rail.&amp;nbsp; The parameters we need are following: 1) Maximum power consumption 2) Peak current&amp;nbsp; 3) Rise time for the +5V input rail during start up BR Gery</description>
      <pubDate>Fri, 09 Apr 2021 17:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Power-consumption/m-p/1259813#M172368</guid>
      <dc:creator>gerassimos_pari</dc:creator>
      <dc:date>2021-04-09T17:01:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM Power consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Power-consumption/m-p/1259935#M172375</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/118732"&gt;@gerassimos_pari&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As for your questions:&lt;/P&gt;
&lt;P&gt;1. That will depend on the application that you are running on the device, you can take a look at the hardware design guide chapter 3.10 Power connectivity/routing. Also please see it on the datasheet chapter 4.1.5 Maximum Supply Currents.&lt;/P&gt;
&lt;P&gt;2. The peak current you can look at the datasheet from the PMIC that we use for the i.MX8QM, please refer to the datasheet.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;3. We do not have an estimated rise time for this, sorry if this may cause you a problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please take a look on the application note that we have for the PMIC, it may help you:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12286.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12286.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Sat, 10 Apr 2021 00:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Power-consumption/m-p/1259935#M172375</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-04-10T00:06:53Z</dc:date>
    </item>
  </channel>
</rss>