<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Configure vsftpd-server on linux OS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/1259305#M172310</link>
    <description>&lt;P&gt;once adding ssl_enable=YES into vsftpd.conf get the following info when launch vsftpd:&lt;BR /&gt;500 OOPS: SSL: ssl_enable is set but SSL support not compiled in.&lt;BR /&gt;&lt;BR /&gt;Per checked, there is openssh and openssl that had been added into local.conf.&lt;BR /&gt;Furthermore, there is libssl.so inside /usr/lib directory in the Linux embedded system.&lt;BR /&gt;&lt;BR /&gt;Modify:&lt;BR /&gt;meta-openembedded/meta-networking/recipes-daemons/vsftpd/vsftpd-3.0.3/nopam-with-tcp_wrapper.patch&lt;BR /&gt;To:&lt;BR /&gt;-#undef VSF_BUILD_SSL&lt;BR /&gt;+#define VSF_BUILD_SSL&lt;BR /&gt;It's not helpful to solve that issue.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Any idea on vsftpd integration?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 09 Apr 2021 03:41:59 GMT</pubDate>
    <dc:creator>adamhuang</dc:creator>
    <dc:date>2021-04-09T03:41:59Z</dc:date>
    <item>
      <title>Configure vsftpd-server on linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/950316#M142103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have included vsftpd-server in my custom linux OS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, I am searching for the configuration of vsftpd-server and vsftpd-client. I want to configure my toradex evaluation board as vsftpd-server and PC as vsftpd-client and want to upload file on vsftpd-server on board and download on vsftpd-client PC.&lt;/P&gt;&lt;P&gt;Can someone help for knowing its configuration!!&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Purvi&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 13:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/950316#M142103</guid>
      <dc:creator>purvi_billore1</dc:creator>
      <dc:date>2019-10-07T13:37:36Z</dc:date>
    </item>
    <item>
      <title>Re: Configure vsftpd-server on linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/950317#M142104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There should not be anything special to i.MX in point of vsftpd configuration.&lt;BR /&gt;It is simply one of FTP server. And optionally it supports SSL.&lt;BR /&gt;You can use vsftpd.conf file for its configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2019 05:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/950317#M142104</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-10-10T05:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: Configure vsftpd-server on linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/1259305#M172310</link>
      <description>&lt;P&gt;once adding ssl_enable=YES into vsftpd.conf get the following info when launch vsftpd:&lt;BR /&gt;500 OOPS: SSL: ssl_enable is set but SSL support not compiled in.&lt;BR /&gt;&lt;BR /&gt;Per checked, there is openssh and openssl that had been added into local.conf.&lt;BR /&gt;Furthermore, there is libssl.so inside /usr/lib directory in the Linux embedded system.&lt;BR /&gt;&lt;BR /&gt;Modify:&lt;BR /&gt;meta-openembedded/meta-networking/recipes-daemons/vsftpd/vsftpd-3.0.3/nopam-with-tcp_wrapper.patch&lt;BR /&gt;To:&lt;BR /&gt;-#undef VSF_BUILD_SSL&lt;BR /&gt;+#define VSF_BUILD_SSL&lt;BR /&gt;It's not helpful to solve that issue.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Any idea on vsftpd integration?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 03:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-vsftpd-server-on-linux-OS/m-p/1259305#M172310</guid>
      <dc:creator>adamhuang</dc:creator>
      <dc:date>2021-04-09T03:41:59Z</dc:date>
    </item>
  </channel>
</rss>