<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bringing up i.MX 6ULL with eMMC and UUU in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1258635#M172240</link>
    <description>&lt;P&gt;Thanks for your reply!&amp;nbsp;&lt;BR /&gt;The PHY was omitted in hardware.&amp;nbsp;&lt;BR /&gt;The reason u-boot was blocking, was not that the PHY was missing, but that it had the wrong address.&lt;/P&gt;</description>
    <pubDate>Thu, 08 Apr 2021 07:23:35 GMT</pubDate>
    <dc:creator>carotte</dc:creator>
    <dc:date>2021-04-08T07:23:35Z</dc:date>
    <item>
      <title>Bringing up i.MX 6ULL with eMMC and UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1256229#M172015</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We recently received our custom board with the i.MX6ULL processor.&lt;/P&gt;&lt;P&gt;It's fairly similar to the EVK, however, one ethernet PHY has been omitted and an eMMC is used instead of the SD card.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, I am having some trouble bringing up the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried using uuu with the provided sample images.&lt;/P&gt;&lt;P&gt;Host terminal:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;sudo ./uuu uuu.auto-imx6ull14x14evk&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.107-15-gd1c466c&lt;/P&gt;&lt;P&gt;Success 0 Failure 0&lt;/P&gt;&lt;P&gt;1:15 &amp;nbsp; 1/ 1 [=================100%=================] SDP: boot -f u-boot-imx6ull14x14evk_emmc.imx&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Board terminal:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 04 2020 - 00:49:03 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX6ULL rev1.1 900 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 51C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (480 x 272)&lt;BR /&gt;.[0] lcdif@21c8000, video&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net: Could not get PHY for FEC1: addr 1&lt;BR /&gt;Could not get PHY for FEC1: addr 1&lt;BR /&gt;Get shared mii bus on &lt;A href="mailto:ethernet@2188000" target="_blank" rel="noopener"&gt;ethernet@2188000&lt;/A&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;It repeats this loop every couple seconds.&lt;/P&gt;&lt;P&gt;Does this mean that not finding the PHY is blocking the next step ?&lt;/P&gt;&lt;P&gt;Any help is appreciated !&lt;/P&gt;</description>
      <pubDate>Fri, 02 Apr 2021 08:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1256229#M172015</guid>
      <dc:creator>carotte</dc:creator>
      <dc:date>2021-04-02T08:45:22Z</dc:date>
    </item>
    <item>
      <title>Bringing up i.MX 6ULL with eMMC and UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1257771#M172178</link>
      <description>&lt;P&gt;how did you omit the phy? did you change the dts file of uboot?&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 08:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1257771#M172178</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-04-07T08:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: Bringing up i.MX 6ULL with eMMC and UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1258635#M172240</link>
      <description>&lt;P&gt;Thanks for your reply!&amp;nbsp;&lt;BR /&gt;The PHY was omitted in hardware.&amp;nbsp;&lt;BR /&gt;The reason u-boot was blocking, was not that the PHY was missing, but that it had the wrong address.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 07:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bringing-up-i-MX-6ULL-with-eMMC-and-UUU/m-p/1258635#M172240</guid>
      <dc:creator>carotte</dc:creator>
      <dc:date>2021-04-08T07:23:35Z</dc:date>
    </item>
  </channel>
</rss>