<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Device mounting problem as mass storage on Windows</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-mounting-problem-as-mass-storage-on-Windows/m-p/1258416#M172223</link>
    <description>&lt;P&gt;Please note that Windows does not support more than one partition on USB flash drive (which is emulated by i.MX board).&lt;/P&gt;</description>
    <pubDate>Thu, 08 Apr 2021 01:17:34 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2021-04-08T01:17:34Z</dc:date>
    <item>
      <title>Device mounting problem as mass storage on Windows</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-mounting-problem-as-mass-storage-on-Windows/m-p/1256505#M172046</link>
      <description>&lt;P&gt;I have downloaded Yocto image in SD Card and created 2 more partitions on the SD card. I am using iMX8mm platform.&lt;/P&gt;&lt;P&gt;I am mounting both the partitions using mass storage module - modprobe g_mass_storage file=/dev/mmcblk1p3,/dev/mmcblk1p5&lt;/P&gt;&lt;P&gt;I was hoping to get both the partitions mounted as mass storage device when connected through USB.&lt;/P&gt;&lt;P&gt;On Windows machine, only one partition being mounted. On Ubuntu machine, both the partitions being mounted.&lt;/P&gt;&lt;P&gt;I am able to mount individual partitions using the following commands&lt;/P&gt;&lt;P&gt;mount /dev/mmcblk1p3 /mnt&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;mount /dev/mmcblk1p5 /mnt&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;They both are FAT32. If I insert the SD Card directly to Windows machine, they mount just fine. And if I mount them one at a time, they both are mounting properly.&lt;/P&gt;&lt;P&gt;Any idea what is going wrong with Windows machine ? How to consistently mount both the partition on all the platforms ?&lt;/P&gt;</description>
      <pubDate>Sun, 04 Apr 2021 16:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-mounting-problem-as-mass-storage-on-Windows/m-p/1256505#M172046</guid>
      <dc:creator>avijitnsec</dc:creator>
      <dc:date>2021-04-04T16:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: Device mounting problem as mass storage on Windows</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-mounting-problem-as-mass-storage-on-Windows/m-p/1258416#M172223</link>
      <description>&lt;P&gt;Please note that Windows does not support more than one partition on USB flash drive (which is emulated by i.MX board).&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 01:17:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-mounting-problem-as-mass-storage-on-Windows/m-p/1258416#M172223</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-04-08T01:17:34Z</dc:date>
    </item>
  </channel>
</rss>