<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error while bitbaking core image on imx gatesgarth distro in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1257784#M172183</link>
    <description>&lt;P&gt;I did nothing but set up MACHINE as imx6ullevk then proceeded to run bitbake core-image-minimal&lt;BR /&gt;&lt;BR /&gt;I did end up getting a working image build from the community distro.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Apr 2021 08:15:17 GMT</pubDate>
    <dc:creator>omerg</dc:creator>
    <dc:date>2021-04-07T08:15:17Z</dc:date>
    <item>
      <title>Error while bitbaking core image on imx gatesgarth distro</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1256501#M172045</link>
      <description>&lt;P&gt;I am building a core image to run on IMX6ULLEVK, and it results in this error:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;| DEBUG: Python function extend_recipe_sysroot finished&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| DEBUG: Executing shell function do_image_wic&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| INFO: Creating image(s)...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;|&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| ERROR: _exec_cmd: install -m 0644 -D /home/dev/imx-yocto-bsp/build/tmp/deploy/images/imx6ullevk/make_dtb_boot_files /home/dev/imx-yocto-bsp/build/tmp/work/imx6ullevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/build-wic/tmp.wic.e0s_evi6/boot.2/make_dtb_boot_files returned '1' instead of 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| output: install: cannot stat '/home/dev/imx-yocto-bsp/build/tmp/deploy/images/imx6ullevk/make_dtb_boot_files': No such file or directory&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;|&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| WARNING: exit code 1 from a shell command.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| ERROR: Execution of '/home/dev/imx-yocto-bsp/build/tmp/work/imx6ullevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/run.do_image_wic.21569' failed with exit code 1:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| INFO: Creating image(s)...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;|&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| ERROR: _exec_cmd: install -m 0644 -D /home/dev/imx-yocto-bsp/build/tmp/deploy/images/imx6ullevk/make_dtb_boot_files /home/dev/imx-yocto-bsp/build/tmp/work/imx6ullevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/build-wic/tmp.wic.e0s_evi6/boot.2/make_dtb_boot_files returned '1' instead of 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| output: install: cannot stat '/home/dev/imx-yocto-bsp/build/tmp/deploy/images/imx6ullevk/make_dtb_boot_files': No such file or directory&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;|&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;| WARNING: exit code 1 from a shell command.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;|&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Now when looking in /tmp/.../imx6ullevk i can see there are files with the exention of .dtb (below are the files that generated in the folder)&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.dtb imx6ull-14x14-evk.dtb&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-btwifi--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.dtb modules--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.tgz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-btwifi-imx6ullevk.dtb modules-imx6ullevk.tgz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-btwifi-oob--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.dtb u-boot-imx-initial-env-imx6ullevk-sd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-btwifi-oob-imx6ullevk.dtb u-boot-imx-initial-env-imx6ullevk-sd-2020.04-r0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-btwifi-oob.dtb u-boot-imx-initial-env-sd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-btwifi.dtb u-boot-imx6ullevk.imx&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-emmc--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.dtb u-boot-imx6ullevk.imx-sd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-emmc-imx6ullevk.dtb u-boot-sd-2020.04-r0.imx&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-emmc.dtb u-boot.imx&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-gpmi-weim--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.dtb u-boot.imx-sd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-gpmi-weim-imx6ullevk.dtb zImage&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-gpmi-weim.dtb zImage--5.10.9+git0+32513c25d8-r0-imx6ullevk-20210404104018.bin&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;imx6ull-14x14-evk-imx6ullevk.dtb zImage-imx6ullevk.bin&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;What can I do to make the image compile? I just need the basic bootable one&lt;/P&gt;</description>
      <pubDate>Sun, 04 Apr 2021 12:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1256501#M172045</guid>
      <dc:creator>omerg</dc:creator>
      <dc:date>2021-04-04T12:58:04Z</dc:date>
    </item>
    <item>
      <title>Re: Error while bitbaking core image on imx gatesgarth distro</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1257775#M172180</link>
      <description>&lt;P&gt;pls give me your bitbake commands step by step, let me check it&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 08:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1257775#M172180</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-04-07T08:05:37Z</dc:date>
    </item>
    <item>
      <title>Re: Error while bitbaking core image on imx gatesgarth distro</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1257784#M172183</link>
      <description>&lt;P&gt;I did nothing but set up MACHINE as imx6ullevk then proceeded to run bitbake core-image-minimal&lt;BR /&gt;&lt;BR /&gt;I did end up getting a working image build from the community distro.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 08:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1257784#M172183</guid>
      <dc:creator>omerg</dc:creator>
      <dc:date>2021-04-07T08:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: Error while bitbaking core image on imx gatesgarth distro</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1259504#M172332</link>
      <description>&lt;P&gt;so you have fixed this issue already?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 08:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-bitbaking-core-image-on-imx-gatesgarth-distro/m-p/1259504#M172332</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-04-09T08:21:47Z</dc:date>
    </item>
  </channel>
</rss>