<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic uImage in Yocto project not generated in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1257774#M172179</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the Yocto project for L3.14.52_1.1.0_ga setup for imx6qsabred board and by running:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake fsl-image-mfgtool-initramfs&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I can see there is zImage_mfgtool generated but no uImage,&lt;BR /&gt;and I added&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;KERNEL_IMAGETYPE = "uImage"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;to imx6qsabresd.conf and manage to generate a uImage.bin file, but not "uImage" which I can use in the mfg tool.&lt;/P&gt;&lt;P&gt;Question:&lt;BR /&gt;1. is the uImage.bin same as "uImage"? Can I use it directly in the mfg tool?&lt;BR /&gt;2. if not, how do I generate a "uImage" file in Yocto project?&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Di&lt;/P&gt;</description>
    <pubDate>Wed, 07 Apr 2021 08:05:27 GMT</pubDate>
    <dc:creator>disheng</dc:creator>
    <dc:date>2021-04-07T08:05:27Z</dc:date>
    <item>
      <title>uImage in Yocto project not generated</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1257774#M172179</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the Yocto project for L3.14.52_1.1.0_ga setup for imx6qsabred board and by running:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake fsl-image-mfgtool-initramfs&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I can see there is zImage_mfgtool generated but no uImage,&lt;BR /&gt;and I added&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;KERNEL_IMAGETYPE = "uImage"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;to imx6qsabresd.conf and manage to generate a uImage.bin file, but not "uImage" which I can use in the mfg tool.&lt;/P&gt;&lt;P&gt;Question:&lt;BR /&gt;1. is the uImage.bin same as "uImage"? Can I use it directly in the mfg tool?&lt;BR /&gt;2. if not, how do I generate a "uImage" file in Yocto project?&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Di&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 08:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1257774#M172179</guid>
      <dc:creator>disheng</dc:creator>
      <dc:date>2021-04-07T08:05:27Z</dc:date>
    </item>
    <item>
      <title>Re: uImage in Yocto project not generated</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1259250#M172302</link>
      <description>&lt;P&gt;why do you need to use uimage? mfgtool can download zimage directly&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 02:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1259250#M172302</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-04-09T02:17:52Z</dc:date>
    </item>
    <item>
      <title>Re: uImage in Yocto project not generated</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1259262#M172303</link>
      <description>&lt;P&gt;Hello Joan,&lt;/P&gt;&lt;P&gt;I figured that out afterwards... Thanks.&lt;/P&gt;&lt;P&gt;Now when we try to use mfgtool to flash, it gets stuck in the kernel and it seems to have unmatched machine id.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="disheng_0-1617934959542.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141776i2C2A0533DB8D6108/image-size/medium?v=v2&amp;amp;px=400" role="button" title="disheng_0-1617934959542.png" alt="disheng_0-1617934959542.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The id passed by uboot is f8c which is correct for imx6q, but the ids in kernel seems strange, all "ffffffff", do you know what can be wrong?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Di&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 02:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uImage-in-Yocto-project-not-generated/m-p/1259262#M172303</guid>
      <dc:creator>disheng</dc:creator>
      <dc:date>2021-04-09T02:25:42Z</dc:date>
    </item>
  </channel>
</rss>