<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLPSPI and DMA Help</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LPSPI-and-DMA-Help/m-p/1256801#M172081</link>
    <description>&lt;P&gt;Hello, I am using the MIMXRT1050 board with Keilv5 Pro edition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a custom project and need help configuring my LPSPI and DMA. My goal is the use DMA to send 160 bytes to the transmit buffer of LPSPI. I have a area of memory where the data is stored. My function will take in the start address of the data and size of data as parameters.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use DMA to send the data to the transmit buffer of the LPSPI. I see there is a special LPSPI_EDMA functions, but I am confused on how to set these API functions for my specific case. All the examples involve a master and slave board. In my case, I will be moving data from memory to the LPSPI TX buffer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is if I use DMA and set the watermark of the FIFO to 2 words, I will be able to send2 words to the transmit buffer then the transmit buffer will be full and send out those words and return empty to take in the next 2 words until the DMA is complete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I use the LPSPI_EDMA to send data from stored memory to the LPSPI TX buffer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Kamal&lt;/P&gt;</description>
    <pubDate>Mon, 05 Apr 2021 20:02:05 GMT</pubDate>
    <dc:creator>kamal1</dc:creator>
    <dc:date>2021-04-05T20:02:05Z</dc:date>
    <item>
      <title>LPSPI and DMA Help</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPSPI-and-DMA-Help/m-p/1256801#M172081</link>
      <description>&lt;P&gt;Hello, I am using the MIMXRT1050 board with Keilv5 Pro edition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a custom project and need help configuring my LPSPI and DMA. My goal is the use DMA to send 160 bytes to the transmit buffer of LPSPI. I have a area of memory where the data is stored. My function will take in the start address of the data and size of data as parameters.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use DMA to send the data to the transmit buffer of the LPSPI. I see there is a special LPSPI_EDMA functions, but I am confused on how to set these API functions for my specific case. All the examples involve a master and slave board. In my case, I will be moving data from memory to the LPSPI TX buffer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is if I use DMA and set the watermark of the FIFO to 2 words, I will be able to send2 words to the transmit buffer then the transmit buffer will be full and send out those words and return empty to take in the next 2 words until the DMA is complete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I use the LPSPI_EDMA to send data from stored memory to the LPSPI TX buffer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Kamal&lt;/P&gt;</description>
      <pubDate>Mon, 05 Apr 2021 20:02:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPSPI-and-DMA-Help/m-p/1256801#M172081</guid>
      <dc:creator>kamal1</dc:creator>
      <dc:date>2021-04-05T20:02:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI and DMA Help</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPSPI-and-DMA-Help/m-p/1259014#M172287</link>
      <description>&lt;P&gt;Hi Kamal,&lt;/P&gt;
&lt;P&gt;I sent you a response to the case you submitted internally about this. If you have any input please let me know.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 16:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPSPI-and-DMA-Help/m-p/1259014#M172287</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-04-08T16:06:51Z</dc:date>
    </item>
  </channel>
</rss>