<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックYocto project host setup</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255607#M171939</link>
    <description>&lt;P&gt;Dear friends ，&lt;/P&gt;&lt;P&gt;I am setting up a host for L5.4... yocto project. Based on the document, I should install package python, pylint3 and rsnc. When I install them, the installer say install pynthon-is-pynth2, git, and pylint should be installed instead of these specified in document . It also say that the package Rsnc can not be located. Is rsnc a typo? &amp;nbsp;Is rsnc should be rsync instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;Hai&lt;/P&gt;</description>
    <pubDate>Thu, 01 Apr 2021 07:30:29 GMT</pubDate>
    <dc:creator>hailiu</dc:creator>
    <dc:date>2021-04-01T07:30:29Z</dc:date>
    <item>
      <title>Yocto project host setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255607#M171939</link>
      <description>&lt;P&gt;Dear friends ，&lt;/P&gt;&lt;P&gt;I am setting up a host for L5.4... yocto project. Based on the document, I should install package python, pylint3 and rsnc. When I install them, the installer say install pynthon-is-pynth2, git, and pylint should be installed instead of these specified in document . It also say that the package Rsnc can not be located. Is rsnc a typo? &amp;nbsp;Is rsnc should be rsync instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;Hai&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 07:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255607#M171939</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2021-04-01T07:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto project host setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255648#M171948</link>
      <description>&lt;P&gt;what ubuntu version do you use? ubuntu 18.04? and send the message or screen shot to me, let me check the detailed information when you install them&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 08:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255648#M171948</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-04-01T08:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto project host setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255663#M171949</link>
      <description>&lt;P&gt;ubuntu 20.04, when I use 20.04, It seems the repo sync has problem. i t give me error like this:&lt;/P&gt;&lt;P&gt;curl: (28) Failed to connect to github.com port 443: Connection timed ou&lt;/P&gt;&lt;P&gt;should I use 18.04?&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 08:43:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255663#M171949</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2021-04-01T08:43:08Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto project host setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255804#M171971</link>
      <description>&lt;P&gt;Dear joan&lt;/P&gt;&lt;P&gt;Switched to 18.04, rsnc still can not be found。I tried to do the repo sync, errors occured. Attanched is a sanpshot.&lt;/P&gt;&lt;P&gt;the following is the error message.&lt;/P&gt;&lt;P&gt;fatal: unable to access '&lt;A href="https://github.com/meta-rust/meta-rust/" target="_blank"&gt;https://github.com/meta-rust/meta-rust/&lt;/A&gt;': Failed to connect to github.com port 443: Connection timed out&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;Hai&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 12:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1255804#M171971</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2021-04-01T12:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto project host setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1256189#M172005</link>
      <description>&lt;P&gt;this is your network connection issue, you need check your network and try again, before you building, don't forget install all of packages in the chapter 3 Host Setup and chapter 1.2.1.&amp;nbsp;Ubuntu and Debian of&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.yoctoproject.org/docs/3.0/ref-manual/ref-manual.html#ubuntu-packages&amp;quot;" target="_blank"&gt;https://www.yoctoproject.org/docs/3.0/ref-manual/ref-manual.html#ubuntu-packages"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;if you forget install something, I suggest that you delete the build folder, install first, then build again&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Apr 2021 07:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-project-host-setup/m-p/1256189#M172005</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-04-02T07:34:08Z</dc:date>
    </item>
  </channel>
</rss>