<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC as Interrupt in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ADC-as-Interrupt/m-p/1253685#M171714</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have configured GPIO1 IO01 as an analog input and are measuring the volatge on that pin using the ADC. We would like to use this pin with the analog input configuration as a wakeup source when the device is in low power mode. Kindly advice on how this can be done.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Akshay Naik&lt;/P&gt;</description>
    <pubDate>Fri, 09 Apr 2021 10:30:18 GMT</pubDate>
    <dc:creator>akshay2528</dc:creator>
    <dc:date>2021-04-09T10:30:18Z</dc:date>
    <item>
      <title>ADC as Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-as-Interrupt/m-p/1253685#M171714</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have configured GPIO1 IO01 as an analog input and are measuring the volatge on that pin using the ADC. We would like to use this pin with the analog input configuration as a wakeup source when the device is in low power mode. Kindly advice on how this can be done.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Akshay Naik&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 10:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-as-Interrupt/m-p/1253685#M171714</guid>
      <dc:creator>akshay2528</dc:creator>
      <dc:date>2021-04-09T10:30:18Z</dc:date>
    </item>
  </channel>
</rss>