<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMax OSPI memory in iMx8 Quad Max</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Max-OSPI-memory-in-iMx8-Quad-Max/m-p/1253496#M171686</link>
    <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;We are in the process of Processor analysis for a project. iMx8 Quad max is one of the major contenders. What is the max OSPI flash supported in iMx8QM. We see chips for up to 2Gb. Will this be supported in iMx8?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 29 Mar 2021 09:40:12 GMT</pubDate>
    <dc:creator>ajmalmali</dc:creator>
    <dc:date>2021-03-29T09:40:12Z</dc:date>
    <item>
      <title>Max OSPI memory in iMx8 Quad Max</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Max-OSPI-memory-in-iMx8-Quad-Max/m-p/1253496#M171686</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;We are in the process of Processor analysis for a project. iMx8 Quad max is one of the major contenders. What is the max OSPI flash supported in iMx8QM. We see chips for up to 2Gb. Will this be supported in iMx8?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 09:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Max-OSPI-memory-in-iMx8-Quad-Max/m-p/1253496#M171686</guid>
      <dc:creator>ajmalmali</dc:creator>
      <dc:date>2021-03-29T09:40:12Z</dc:date>
    </item>
    <item>
      <title>Re: Max OSPI memory in iMx8 Quad Max</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Max-OSPI-memory-in-iMx8-Quad-Max/m-p/1253530#M171692</link>
      <description>&lt;P&gt;Hi Ajmal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at Table 5-19. FlexSPI Configuration block&lt;/P&gt;
&lt;P&gt;sflashA1Size&amp;nbsp; 4bytes&amp;nbsp;&amp;nbsp; -..actual size, in terms of bytes&amp;nbsp; (the same is for i.MX8QM)&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 10:32:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Max-OSPI-memory-in-iMx8-Quad-Max/m-p/1253530#M171692</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-29T10:32:11Z</dc:date>
    </item>
  </channel>
</rss>