<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8MQ6 BSDL/ID Code mismatch</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ6-BSDL-ID-Code-mismatch/m-p/1252312#M171493</link>
    <description>&lt;P&gt;Hello I hope someone can help!&lt;/P&gt;&lt;P&gt;I have a IMX8MQ6CVAHZAB populated twice on my pcba. (TDI = W5, TDO = U5).&lt;/P&gt;&lt;P&gt;When sniffing the device with jtaglive it reads the 'freescale' ID code as 00001000100011100010000000011101&lt;/P&gt;&lt;P&gt;This matches the user manual description of the SJC ID Code&lt;/P&gt;&lt;P&gt;However the BSDL file (IMX8M) lists the ID Code as 00011100111110000000010101010011&lt;/P&gt;&lt;P&gt;JTAG Mod is high, and only one core is detected.&lt;/P&gt;&lt;P&gt;I am also confident the other pins are as per the compliance section.&lt;/P&gt;&lt;P&gt;Can anyone advise if there is a different BSDL file I should be using?&lt;/P&gt;&lt;P&gt;Thanks Ian&lt;/P&gt;</description>
    <pubDate>Thu, 25 Mar 2021 16:52:46 GMT</pubDate>
    <dc:creator>ians1</dc:creator>
    <dc:date>2021-03-25T16:52:46Z</dc:date>
    <item>
      <title>IMX8MQ6 BSDL/ID Code mismatch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ6-BSDL-ID-Code-mismatch/m-p/1252312#M171493</link>
      <description>&lt;P&gt;Hello I hope someone can help!&lt;/P&gt;&lt;P&gt;I have a IMX8MQ6CVAHZAB populated twice on my pcba. (TDI = W5, TDO = U5).&lt;/P&gt;&lt;P&gt;When sniffing the device with jtaglive it reads the 'freescale' ID code as 00001000100011100010000000011101&lt;/P&gt;&lt;P&gt;This matches the user manual description of the SJC ID Code&lt;/P&gt;&lt;P&gt;However the BSDL file (IMX8M) lists the ID Code as 00011100111110000000010101010011&lt;/P&gt;&lt;P&gt;JTAG Mod is high, and only one core is detected.&lt;/P&gt;&lt;P&gt;I am also confident the other pins are as per the compliance section.&lt;/P&gt;&lt;P&gt;Can anyone advise if there is a different BSDL file I should be using?&lt;/P&gt;&lt;P&gt;Thanks Ian&lt;/P&gt;</description>
      <pubDate>Thu, 25 Mar 2021 16:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ6-BSDL-ID-Code-mismatch/m-p/1252312#M171493</guid>
      <dc:creator>ians1</dc:creator>
      <dc:date>2021-03-25T16:52:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ6 BSDL/ID Code mismatch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ6-BSDL-ID-Code-mismatch/m-p/1252523#M171523</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149236"&gt;@ians1&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Please check if Your configuration satisfies COMPLIANCE_PATTERNS&lt;BR /&gt;in the BSDL file.&lt;/P&gt;
&lt;P&gt;attribute COMPLIANCE_PATTERNS of IMX8M: entity is &lt;BR /&gt;"(BOOT_MODE0, BOOT_MODE1, GPIO1_IO00, GPIO1_IO01, GPIO1_IO02, " &amp;amp;&lt;BR /&gt;"GPIO1_IO03, TEST_MODE) (0000011)";&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX8M_BSDL" target="_blank"&gt;https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX8M_BSDL&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Also:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Entering-Boundary-Scan-mode/m-p/915500#M137832" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Entering-Boundary-Scan-mode/m-p/915500&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 03:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ6-BSDL-ID-Code-mismatch/m-p/1252523#M171523</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-03-26T03:29:44Z</dc:date>
    </item>
  </channel>
</rss>