<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX27 Board is not Flashing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX27-Board-is-not-Flashing/m-p/230252#M17139</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using IMX27 (MCIMX27VOP4A-M72J-CTAM1325Z)&lt;/P&gt;&lt;P&gt;processor &amp;amp; PMIC-MC13783VK5 for G3 project. We need to&lt;/P&gt;&lt;P&gt;program the NOR flash(S29GL256N) using serial port(UART)&lt;/P&gt;&lt;P&gt;in our G3 board using Advanced tool kit(ATK). Some of the&lt;/P&gt;&lt;P&gt;boards are not able to program the NOR flash. I have&lt;/P&gt;&lt;P&gt;mentioned below the error showing on ATK Window while&lt;/P&gt;&lt;P&gt;programming the NOR flash.I have attached the Images.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Also , Some of the boards are suddenly got failed after 3-4 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;moths.After that , those boards are not able to re-flash &amp;amp; boot&lt;/P&gt;&lt;P&gt;( Initially Passed Boards).Those failed boards are impedance&lt;/P&gt;&lt;P&gt;&amp;amp; voltages,Clocks are proper.&lt;/P&gt;&lt;P&gt;Please suggest your Input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below i have mentioned issues while flashing.&lt;/P&gt;&lt;P&gt;1)Can't execute RAM kernal.&lt;/P&gt;&lt;P&gt;2)Connection error. Please reset the board and make sure the&lt;/P&gt;&lt;P&gt;board in&lt;/P&gt;&lt;P&gt;bootstrap mode.(Most of the time showing this issue)&lt;/P&gt;&lt;P&gt;3)Reset the target.&lt;/P&gt;&lt;P&gt;Note : While Flashing boards are in bootstrap mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Azlum&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Oct 2013 10:15:32 GMT</pubDate>
    <dc:creator>mohammedazlum</dc:creator>
    <dc:date>2013-10-24T10:15:32Z</dc:date>
    <item>
      <title>IMX27 Board is not Flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX27-Board-is-not-Flashing/m-p/230252#M17139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using IMX27 (MCIMX27VOP4A-M72J-CTAM1325Z)&lt;/P&gt;&lt;P&gt;processor &amp;amp; PMIC-MC13783VK5 for G3 project. We need to&lt;/P&gt;&lt;P&gt;program the NOR flash(S29GL256N) using serial port(UART)&lt;/P&gt;&lt;P&gt;in our G3 board using Advanced tool kit(ATK). Some of the&lt;/P&gt;&lt;P&gt;boards are not able to program the NOR flash. I have&lt;/P&gt;&lt;P&gt;mentioned below the error showing on ATK Window while&lt;/P&gt;&lt;P&gt;programming the NOR flash.I have attached the Images.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Also , Some of the boards are suddenly got failed after 3-4 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;moths.After that , those boards are not able to re-flash &amp;amp; boot&lt;/P&gt;&lt;P&gt;( Initially Passed Boards).Those failed boards are impedance&lt;/P&gt;&lt;P&gt;&amp;amp; voltages,Clocks are proper.&lt;/P&gt;&lt;P&gt;Please suggest your Input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below i have mentioned issues while flashing.&lt;/P&gt;&lt;P&gt;1)Can't execute RAM kernal.&lt;/P&gt;&lt;P&gt;2)Connection error. Please reset the board and make sure the&lt;/P&gt;&lt;P&gt;board in&lt;/P&gt;&lt;P&gt;bootstrap mode.(Most of the time showing this issue)&lt;/P&gt;&lt;P&gt;3)Reset the target.&lt;/P&gt;&lt;P&gt;Note : While Flashing boards are in bootstrap mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Azlum&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2013 10:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX27-Board-is-not-Flashing/m-p/230252#M17139</guid>
      <dc:creator>mohammedazlum</dc:creator>
      <dc:date>2013-10-24T10:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: IMX27 Board is not Flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX27-Board-is-not-Flashing/m-p/230253#M17140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like memory (of i.MX27) is not working (or not initialyzed correctly)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2013 08:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX27-Board-is-not-Flashing/m-p/230253#M17140</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-10-25T08:30:26Z</dc:date>
    </item>
  </channel>
</rss>