<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Demo Framework</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251246#M171382</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;The demo framework for Yocto is per default only compatible with the BSP it was released with. Since the BSP is responsible for supplying any third-party libraries the demo framework depends upon. This is the only version that has been tested on a given BSP. Since the build is not finding a 'BSP supplied' header file it means that either the BSP is not compatible with that version of the demo framework or the environment is not configured correctly.&lt;/P&gt;
&lt;P&gt;In general, its only recommended to use the version compatible with your current BSP.&lt;/P&gt;
&lt;P&gt;But if you want to experiment with an unsupported version it ought to be possible to run a newer demo framework like the latest release from github on most BSP's by either "manually providing all required dependencies" or by adding "--Recipes [*]" to your build command. Beware that the recipes parameter only downloads 'header only' dependencies so any new library dependencies will not be downloaded. Furthermore using "--Recipes" might download header files already present in your BSP image in different versions with could lead to "interesting" compile issues. If the "--Recipes" parameter don’t work you can try the manual solution and you can look in the "ThirdParty\Recipe" folder to see which third party libraries we require and you can get an idea of how we build them for other platforms. &lt;SPAN&gt;But since you are running it on an untested BSP that comes with older versions of various libraries you might encounter various issues.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards, René&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Mar 2021 12:51:30 GMT</pubDate>
    <dc:creator>renethrane-b494</dc:creator>
    <dc:date>2021-03-24T12:51:30Z</dc:date>
    <item>
      <title>Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1163354#M162967</link>
      <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;Hello,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;We are referring i.MX Graphics User’s Guide to developing a graphical application (IMXGRAPHICUG Rev. 6, 06/2020). We are referring to Chapter 17 Demo Framework for creating the graphical application.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;We followed the Building using a full Yocto build steps, the only difference is that we have used distro x-Wayland and core-image-base for building our kernel and rootfs.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;For compiling sample we are using&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;&lt;STRONG&gt;cd DemoApps/GLES2/S06_Texturing &lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;&lt;STRONG&gt;FslBuild.py --Variants [WindowSystem=Wayland] &lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;Then we are getting the error about the as follows&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;&lt;SPAN&gt;../../../../DemoFramework/FslBase/include/FslBase/Log/IO/FmtPath.hpp:35:10: fatal error: fmt/format.h: No such file or directory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;35 | #include &amp;lt;fmt/format.h&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;| &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;^~~~~~~~~~~~~~&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;compilation terminated.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;So, these files are to be present in the demo framework or need to add to build successfully. &lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;The demo framework is getting from the this &lt;A href="https://github.com/NXPmicro/gtec-demo-framework" target="_self"&gt;link&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Oct 2020 10:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1163354#M162967</guid>
      <dc:creator>barish_malshika</dc:creator>
      <dc:date>2020-10-06T10:55:42Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1163424#M162980</link>
      <description>&lt;P&gt;Hello barish,&lt;/P&gt;
&lt;DIV class="lia-quilt-column lia-quilt-column-24 lia-quilt-column-single lia-quilt-column-message-body-content"&gt;
&lt;DIV class="lia-quilt-column-alley lia-quilt-column-alley-single"&gt;
&lt;DIV class="lia-panel lia-panel-standard MessageTagsTaplet Chrome lia-component-message-view-widget-tags"&gt;
&lt;DIV class="lia-decoration-border"&gt;
&lt;DIV class="lia-decoration-border-content"&gt;
&lt;DIV&gt;
&lt;DIV class="lia-panel-content-wrapper"&gt;
&lt;DIV class="lia-panel-content"&gt;
&lt;DIV class="AddMessageTags lia-message-tags"&gt;&lt;A id="showAddTag_1" class="lia-link-navigation add-tag-link" href="https://community.nxp.com/t5/i-MX-Processors/gtec-demo-framework-Error-Missing-installation-of-package-xx-and/td-p/893672#" aria-label="Add Tag..." target="_blank"&gt;&lt;/A&gt;
&lt;P&gt;This is a known issue.&amp;nbsp;If you are using a old version of the SDK that doesn't come with all required third party software you will need to add --Recipes [*] to your build command as that will re-enable the download.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can see more information on the known issues page:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXPmicro/gtec-demo-framework/blob/master/KnownIssues.md" rel="nofollow noopener noreferrer" target="_blank"&gt;https://github.com/NXPmicro/gtec-demo-framework/blob/master/KnownIssues.md&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope this helps!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 06 Oct 2020 13:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1163424#M162980</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-10-06T13:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1242843#M170588</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;SPAN class=""&gt;Bio_TICFSL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Recently, I had &lt;STRONG&gt;same trouble&lt;/STRONG&gt;... please tell me the using correctly method.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;frist&lt;/STRONG&gt;,&lt;/P&gt;&lt;P&gt;I build a Yocto Project and runqemu-extract this image.tar.bz2 file ($ bitbake imx-image-full )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;second, &lt;/STRONG&gt;set up envirnoment&lt;BR /&gt;source prepare.sh&lt;BR /&gt;source ~/sdk/.../5.4-zeus/environment-setup-aarch64-poky-linux&lt;BR /&gt;export FSL_PLATFORM_NAME=Yocto&lt;BR /&gt;export ROOTFS=~/i.mx8-yocto-image-zip-folder&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;final,&amp;nbsp;&lt;/STRONG&gt; build DEMO APP&lt;/P&gt;&lt;P&gt;FslBuild.py --Variants [WindowSystem=Wayland] -c install --CMakeInstallPrefix $FSL_GRAPHICS_SDK/bin --Recipes [*]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error :&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;error: fmt/format.h: No such file or directory&lt;BR /&gt;#include &amp;lt;fmt/format.h&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could you tell me which step of wrong ?? thank Your help.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Weilly Li&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 02:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1242843#M170588</guid>
      <dc:creator>weilly_li</dc:creator>
      <dc:date>2021-03-10T02:24:50Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1249707#M171213</link>
      <description>&lt;P&gt;Dear &lt;SPAN class=""&gt;Bio_TICFSL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I am also facing the same issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN class=""&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;DemoFramework/FslBase/include/FslBase/Log/IO/FmtPath.hpp:35:10: fatal error: fmt/format.h: No such file or directory&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN class=""&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;#include &amp;lt;fmt/format.h&amp;gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;&lt;BR /&gt;&lt;SPAN&gt;compilation terminated.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;&lt;SPAN&gt;Pls suggest us&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN class=""&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;Regards&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3" color="#000000"&gt;&lt;SPAN&gt;Ramesh&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 13:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1249707#M171213</guid>
      <dc:creator>RameshChandrakasan</dc:creator>
      <dc:date>2021-03-22T13:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251246#M171382</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;The demo framework for Yocto is per default only compatible with the BSP it was released with. Since the BSP is responsible for supplying any third-party libraries the demo framework depends upon. This is the only version that has been tested on a given BSP. Since the build is not finding a 'BSP supplied' header file it means that either the BSP is not compatible with that version of the demo framework or the environment is not configured correctly.&lt;/P&gt;
&lt;P&gt;In general, its only recommended to use the version compatible with your current BSP.&lt;/P&gt;
&lt;P&gt;But if you want to experiment with an unsupported version it ought to be possible to run a newer demo framework like the latest release from github on most BSP's by either "manually providing all required dependencies" or by adding "--Recipes [*]" to your build command. Beware that the recipes parameter only downloads 'header only' dependencies so any new library dependencies will not be downloaded. Furthermore using "--Recipes" might download header files already present in your BSP image in different versions with could lead to "interesting" compile issues. If the "--Recipes" parameter don’t work you can try the manual solution and you can look in the "ThirdParty\Recipe" folder to see which third party libraries we require and you can get an idea of how we build them for other platforms. &lt;SPAN&gt;But since you are running it on an untested BSP that comes with older versions of various libraries you might encounter various issues.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards, René&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 12:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251246#M171382</guid>
      <dc:creator>renethrane-b494</dc:creator>
      <dc:date>2021-03-24T12:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251249#M171384</link>
      <description>&lt;P&gt;Dear &lt;SPAN class=""&gt;Bio TICFSL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;As per your suggestions SDK by us to build Demoframe work is old..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;But, As per the yocto image build recipe&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#00FF00"&gt;&lt;SPAN class=""&gt;[DISTRO=fsl-imx-wayland MACHINE=imx8qmmek source imx-setup-release.sh -b build-wayland]&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN class=""&gt;sources/meta-imx/meta-sdk/recipes-graphics/imx-gpu-sdk/imx-gpu-sdk_5.6.1.bb&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN class=""&gt;I am also using imx-gpu-sdk_5.6.1.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN class=""&gt;Then, Pls suggest what more wrong with graphics driver.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN class=""&gt;Ramesh&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 12:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251249#M171384</guid>
      <dc:creator>RameshChandrakasan</dc:creator>
      <dc:date>2021-03-24T12:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251258#M171385</link>
      <description>&lt;P&gt;&lt;STRONG&gt;&lt;FONT color="#FF6600"&gt;Dear Rene&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#008000"&gt;Thanks, Your are rightly pointed out.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;As per your suggestions SDK by us to build DemoFrame work match with BSP version.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;But, As per the yocto image build recipe&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;[DISTRO=fsl-imx-wayland MACHINE=imx8qmmek source imx-setup-release.sh -b build-wayland]&lt;/P&gt;&lt;P&gt;sources/meta-imx/meta-sdk/recipes-graphics/imx-gpu-sdk/imx-gpu-sdk_5.6.1.bb&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;So,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;I am also using imx-gpu-sdk_5.6.1.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Then, Pls suggest what more wrong with graphics driver.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ramesh&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 13:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251258#M171385</guid>
      <dc:creator>RameshChandrakasan</dc:creator>
      <dc:date>2021-03-24T13:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251265#M171386</link>
      <description>&lt;P&gt;Dear Rene&lt;/P&gt;&lt;P&gt;&lt;FONT color="#008000"&gt;As per your suggestions ,BSP version should match with DemoFrame work binary&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;But, As per the yocto image build recipe&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;[DISTRO=fsl-imx-wayland MACHINE=imx8qmmek source imx-setup-release.sh -b build-wayland]&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;sources/meta-imx/meta-sdk/recipes-graphics/imx-gpu-sdk/imx-gpu-sdk_5.6.1.bb&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT color="#FF00FF"&gt;So, fmt/format.h missing issue is coming&lt;BR /&gt;&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am also using imx-gpu-sdk_5.6.1.&lt;/P&gt;&lt;P&gt;Then also&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Then, Pls suggest what more wrong with graphics driver.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ramesh&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-link-navigation child-thread lia-link-disabled"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 13:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1251265#M171386</guid>
      <dc:creator>RameshChandrakasan</dc:creator>
      <dc:date>2021-03-24T13:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1268090#M173195</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the delayed response..&amp;nbsp; If you are still encountering a fmt.h header file missing erorr, it would seem to suggest&lt;/P&gt;
&lt;P&gt;1. You are not building the demo framework that came with the BSP, since the BSP should include all necessary files.&lt;/P&gt;
&lt;P&gt;2. You did not configure the build environment correct, make sure that your rootfs contains the fmt.h header file and library (which it ought to contain if step 1 is true).&lt;/P&gt;
&lt;P&gt;3. The specific BSP release is missing a key file (this is unlikely but possible).&lt;/P&gt;
&lt;P&gt;Since its not finding the fmt library its very likely that more required packages are missing from the image you are currently using.&lt;/P&gt;
&lt;P&gt;Did you follow the instructions in "DemoFramework\Doc\Setup_guide_yocto.md" specifically "Building using a full Yocto build"?&lt;/P&gt;
&lt;P&gt;As a workaround you can manually build the fmt library and add it to your rootfs.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 10:26:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1268090#M173195</guid>
      <dc:creator>renethrane-b494</dc:creator>
      <dc:date>2021-04-26T10:26:26Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1391927#M185011</link>
      <description>&lt;P&gt;i want to build it in Eclipse IDE? please come out step by step how to setup to build demo in Eclipse IDE i cannot find any document for help??&lt;/P&gt;</description>
      <pubDate>Sun, 26 Dec 2021 01:18:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1391927#M185011</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2021-12-26T01:18:53Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1391950#M185019</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We do not officially support Eclipse as a IDE. But &lt;U&gt;you might&lt;/U&gt; get it working by using a command like&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FslBuildGen.py --CMakeGeneratorName "Eclipse CDT4 - Ninja"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suspect that would work like any other cmake generated Eclipse project so you should be able to google for help on that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But again beware we do not test that backend nor do we officially support it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards, René&lt;/P&gt;</description>
      <pubDate>Sun, 26 Dec 2021 11:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1391950#M185019</guid>
      <dc:creator>renethrane-b494</dc:creator>
      <dc:date>2021-12-26T11:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: Demo Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1392164#M185058</link>
      <description>&lt;P&gt;hi all, i used&amp;nbsp;&lt;SPAN&gt;multimedia&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;bitbake imx-image-multimedia&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;this Build in command line is&amp;nbsp; quick easy steps as 123 :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;0 linux git clone the repo :git clone &lt;A href="https://github.com/NXPmicro/gtec-demo-framework.git" target="_blank" rel="noopener"&gt;https://github.com/NXPmicro/gtec-demo-framework.git&lt;/A&gt;&lt;/P&gt;&lt;P&gt;1 yocto toolchain environments setup:&amp;nbsp;&lt;SPAN&gt;source /opt/fsl-imx-xwayland/5.10-hardknott/environment-setup-cortexa35-poky-linux&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2&lt;EM&gt;&lt;STRONG&gt; at the root dir of the demo&lt;/STRONG&gt;&lt;/EM&gt; , source prepare.sh&amp;nbsp;&lt;/P&gt;&lt;P&gt;3 &lt;EM&gt;&lt;STRONG&gt;at the demo apps dir&lt;/STRONG&gt; &lt;/EM&gt;, build it ok ,&amp;nbsp;&lt;SPAN&gt;FslBuild.py --Variants [WindowSystem=Wayland]&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;please see:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Fslbuild-py-error-usr-bin-env-python3-r-No-such-file-or/td-p/1391938" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/Fslbuild-py-error-usr-bin-env-python3-r-No-such-file-or/td-p/1391938&lt;/A&gt;&lt;/P&gt;&lt;P&gt;thank you all&lt;/P&gt;&lt;P&gt;Joseph zhou jian hui&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 05:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Demo-Framework/m-p/1392164#M185058</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2021-12-28T05:13:08Z</dc:date>
    </item>
  </channel>
</rss>