<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8QM MEK input/output GPIO settings</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1250023#M171238</link>
    <description>&lt;P&gt;Hi support,&lt;/P&gt;&lt;P&gt;I'd like to validate iMX8QM MEK input GPIO pins using uboot-imx (5.4.70_2.3.0).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can we use FGPIO APIs from uboot-imx ?&lt;/LI&gt;&lt;LI&gt;Is it possible to read the boot mode dip switch (SW2) pins for this ?&lt;/LI&gt;&lt;LI&gt;If not SW2, which input GPIO pins on the MEK can be used to test this ? Any examples ?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Ravi&lt;/P&gt;</description>
    <pubDate>Tue, 23 Mar 2021 03:29:14 GMT</pubDate>
    <dc:creator>rkohli2000</dc:creator>
    <dc:date>2021-03-23T03:29:14Z</dc:date>
    <item>
      <title>iMX8QM MEK input/output GPIO settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1250023#M171238</link>
      <description>&lt;P&gt;Hi support,&lt;/P&gt;&lt;P&gt;I'd like to validate iMX8QM MEK input GPIO pins using uboot-imx (5.4.70_2.3.0).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can we use FGPIO APIs from uboot-imx ?&lt;/LI&gt;&lt;LI&gt;Is it possible to read the boot mode dip switch (SW2) pins for this ?&lt;/LI&gt;&lt;LI&gt;If not SW2, which input GPIO pins on the MEK can be used to test this ? Any examples ?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Ravi&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 03:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1250023#M171238</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2021-03-23T03:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM MEK input/output GPIO settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1250049#M171244</link>
      <description>&lt;P&gt;SW2 is not GPIO. it is boot mode pin. not a GPIO.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the GPIO you can run the gpio command in uboot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Untitled.png" style="width: 785px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140331i924B61F5A63F1810/image-size/large?v=v2&amp;amp;px=999" role="button" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 04:05:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1250049#M171244</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2021-03-23T04:05:44Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM MEK input/output GPIO settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1254350#M171805</link>
      <description>&lt;P&gt;Hi Biyong, Please ignore this comment below. I found the issue. Thanks for the reply.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ravi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;Hi Biyong,&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;I'm using uboot-imx_5.4.70_2.3.0 under the imx8QM MEK board. I can see imx8qm_mek_defconfig shows "CONFIG_CMD_GPIO=y". But, there is no gpio supported on the CLI.&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;Is it supported in BSP 5.4.70_2.3.0 ? Or any known MEK driver fixes or patch to support the basic command ?&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;Thanks.&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;BuildInfo:&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;- SCFW 0d54291f, SECO-FW d63fdb21, IMX-MKIMAGE b392ccaa, ATF&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;- U-Boot 2021.00&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;switch to partitions #0, OK&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;mmc0(part 0) is current device&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;flash target is MMC:0&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Net:&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Warning: ethernet@5b040000 using MAC address from ROM&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;eth0: ethernet@5b040000 [PRIME]&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Warning: ethernet@5b050000 using MAC address from ROM&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;, eth1: ethernet@5b050000&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Fastboot: Normal&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Normal Boot&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Hit any key to stop autoboot: 0&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;=&amp;gt;&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;=&amp;gt;&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;=&amp;gt; gpio status&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;Unknown command 'gpio' - try 'help'&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;&lt;FONT face="courier new,courier" size="2"&gt;=&amp;gt;&lt;/FONT&gt;&lt;/STRIKE&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 18:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-input-output-GPIO-settings/m-p/1254350#M171805</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2021-03-30T18:53:15Z</dc:date>
    </item>
  </channel>
</rss>