<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FlashLoader for 1021? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1249625#M171209</link>
    <description>&lt;P&gt;The m_text size is set to what is available for this chip. I can get the software to build by building for release, but I was hoping to be able to build for debug and print to the debug console. The release code runs as expected. Again, I was hoping to be able to interact with the board more with debug features.&lt;/P&gt;</description>
    <pubDate>Mon, 22 Mar 2021 10:59:15 GMT</pubDate>
    <dc:creator>JesseCronce</dc:creator>
    <dc:date>2021-03-22T10:59:15Z</dc:date>
    <item>
      <title>FlashLoader for 1021?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1245236#M170818</link>
      <description>&lt;P&gt;Hello! I downloaded the flashloader application as a starting point for a custom bootloader for a 1021 project. When I try to build the example loader I get&lt;/P&gt;&lt;P&gt;section `.text' will not fit in region `m_text'&lt;BR /&gt;m_text: 96280 B 87 KB &lt;FONT color="#FF6600"&gt;108.07%&lt;/FONT&gt;&lt;BR /&gt;c:/nxp/mcuxpressoide_11.1.0_3209/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.1.0.201909161352/tools/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld.exe: region `m_text' overflowed by 7192 bytes&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Is there a different or updated version of a bootloader/flash writer that will build for this processor? I have to make modifications to this application anyway, but I would prefer to start with a working image if I could and make changes from there. I would have hoped the example projects would build.&lt;/P&gt;&lt;P&gt;Also, is there any sort of application guide for this software? I found a few posts on the topic, but if there was something in the way of a usage or commissioning or application manual, that would be such a help to me!&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Sun, 14 Mar 2021 15:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1245236#M170818</guid>
      <dc:creator>JesseCronce</dc:creator>
      <dc:date>2021-03-14T15:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: FlashLoader for 1021?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1246773#M170939</link>
      <description>&lt;P&gt;Please try to increase m_text region size in linker file.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 02:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1246773#M170939</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-03-17T02:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: FlashLoader for 1021?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1249625#M171209</link>
      <description>&lt;P&gt;The m_text size is set to what is available for this chip. I can get the software to build by building for release, but I was hoping to be able to build for debug and print to the debug console. The release code runs as expected. Again, I was hoping to be able to interact with the board more with debug features.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 10:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlashLoader-for-1021/m-p/1249625#M171209</guid>
      <dc:creator>JesseCronce</dc:creator>
      <dc:date>2021-03-22T10:59:15Z</dc:date>
    </item>
  </channel>
</rss>