<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックyocto firmware</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-firmware/m-p/1248824#M171130</link>
    <description>I got the following error when building Yocto: WARNING: firmware-imx-1_5.4-r0 do_fetch: Failed to fetch URL git://github.com/NXP/imx-firmware.git;protocol=https;branch=master;destsuffix=imx-firmware;name=imx-firmware, attempting MIRRORS if available ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output: Cloning into bare repository '/home/zxs/bin/imx-yocto-bsp/downloads//git2/github.com.NXP.imx-firmware.git'... fatal: unable to access '&lt;A href="https://github.com/NXP/imx-firmware.git/" target="_blank"&gt;https://github.com/NXP/imx-firmware.git/&lt;/A&gt;': gnutls_handshake() failed: Error in the pull function. ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://github.com/NXP/imx-firmware.git;protocol=https;branch=master;destsuffix=imx-firmware;name=imx-firmware'. Unable to fetch URL from any source. ERROR: Logfile of failure stored in: /home/zxs/bin/imx-yocto-bsp/build/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/firmware-imx/1_5.4-r0/temp/log.do_fetch.125506 ERROR: Task 1414 (/home/zxs/bin/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_5.4.bb, do_fetch) failed with exit code '1' NOTE: Tasks Summary: Attempted 7734 tasks of which 7733 didn't need to be rerun and 1 failed. No currently running tasks (3908 of 7756) Summary: 1 task failed: /home/zxs/bin/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_5.4.bb, do_fetch Summary: There were 2 WARNING messages shown. Summary: There were 2 ERROR messages shown, returning a non-zero exit code. I found a post on the forum and modified it according to the above, but the same error still appeared. The post is as follows: &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/unable-to-connect-to-git-freescale-com/ta-p/1104028" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/unable-to-connect-to-git-freescale-com/ta-p/1104028&lt;/A&gt; I found that the download site was changed from git://git.freescale.com/imx/imx-firmware.git to git://github.com/NXP/imx-firmware.git. I downloaded it manually from git://github.com/NXP/imx-firmware.git. But it still doesn't work. Can anyone help me</description>
    <pubDate>Fri, 19 Mar 2021 09:59:06 GMT</pubDate>
    <dc:creator>2548903578</dc:creator>
    <dc:date>2021-03-19T09:59:06Z</dc:date>
    <item>
      <title>yocto firmware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-firmware/m-p/1248824#M171130</link>
      <description>I got the following error when building Yocto: WARNING: firmware-imx-1_5.4-r0 do_fetch: Failed to fetch URL git://github.com/NXP/imx-firmware.git;protocol=https;branch=master;destsuffix=imx-firmware;name=imx-firmware, attempting MIRRORS if available ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output: Cloning into bare repository '/home/zxs/bin/imx-yocto-bsp/downloads//git2/github.com.NXP.imx-firmware.git'... fatal: unable to access '&lt;A href="https://github.com/NXP/imx-firmware.git/" target="_blank"&gt;https://github.com/NXP/imx-firmware.git/&lt;/A&gt;': gnutls_handshake() failed: Error in the pull function. ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://github.com/NXP/imx-firmware.git;protocol=https;branch=master;destsuffix=imx-firmware;name=imx-firmware'. Unable to fetch URL from any source. ERROR: Logfile of failure stored in: /home/zxs/bin/imx-yocto-bsp/build/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/firmware-imx/1_5.4-r0/temp/log.do_fetch.125506 ERROR: Task 1414 (/home/zxs/bin/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_5.4.bb, do_fetch) failed with exit code '1' NOTE: Tasks Summary: Attempted 7734 tasks of which 7733 didn't need to be rerun and 1 failed. No currently running tasks (3908 of 7756) Summary: 1 task failed: /home/zxs/bin/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_5.4.bb, do_fetch Summary: There were 2 WARNING messages shown. Summary: There were 2 ERROR messages shown, returning a non-zero exit code. I found a post on the forum and modified it according to the above, but the same error still appeared. The post is as follows: &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/unable-to-connect-to-git-freescale-com/ta-p/1104028" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/unable-to-connect-to-git-freescale-com/ta-p/1104028&lt;/A&gt; I found that the download site was changed from git://git.freescale.com/imx/imx-firmware.git to git://github.com/NXP/imx-firmware.git. I downloaded it manually from git://github.com/NXP/imx-firmware.git. But it still doesn't work. Can anyone help me</description>
      <pubDate>Fri, 19 Mar 2021 09:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-firmware/m-p/1248824#M171130</guid>
      <dc:creator>2548903578</dc:creator>
      <dc:date>2021-03-19T09:59:06Z</dc:date>
    </item>
  </channel>
</rss>