<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using MINISASTOCSI camera module with i.MX 8QuadMax MEK CPU Board (imx8qmmek) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-MINISASTOCSI-camera-module-with-i-MX-8QuadMax-MEK-CPU/m-p/1247481#M170996</link>
    <description>&lt;P&gt;I figured out what the problem was, I was trying to use the wrong device tree file.&amp;nbsp; I changed it to&amp;nbsp;&lt;/P&gt;&lt;P&gt;setenv &lt;SPAN&gt;fdt_file&amp;nbsp;&lt;/SPAN&gt;imx8qm-mek-ov5640.dtb&lt;/P&gt;&lt;P&gt;The system then was able to load the camera.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can be closed.&lt;/P&gt;</description>
    <pubDate>Wed, 17 Mar 2021 17:57:07 GMT</pubDate>
    <dc:creator>amberworth</dc:creator>
    <dc:date>2021-03-17T17:57:07Z</dc:date>
    <item>
      <title>Using MINISASTOCSI camera module with i.MX 8QuadMax MEK CPU Board (imx8qmmek)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MINISASTOCSI-camera-module-with-i-MX-8QuadMax-MEK-CPU/m-p/1246648#M170933</link>
      <description>&lt;P&gt;I'm trying to get the MINISASTOCSI camera module to work with the i.MX 8QuadMax MEK CPU board.&lt;/P&gt;&lt;P&gt;I've connected the SAS plug from J10 (CSI0?) to the MIPICSI camera.&lt;/P&gt;&lt;P&gt;I'm loading it with an imx-image-full yocto build.&lt;/P&gt;&lt;P&gt;After linux boot, the camera is not showing up. (no video sources show&amp;nbsp; when I run&amp;nbsp;&amp;nbsp;gst-device-monitor-1.0)&lt;/P&gt;&lt;P&gt;Things I've tried:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Making sure that the SAS connector is well seated on both sides (audible clicks)&lt;/LI&gt;&lt;LI&gt;Connecting to J5 (CSI1?).&amp;nbsp; This made no difference.&lt;/LI&gt;&lt;LI&gt;Stopping at uboot and trying "setenv fdt_file fsl-imx-evk-mipi-csi2.dtb". This ended up breaking the device tree. When I tried to start linux with&amp;nbsp;run bootcmd, I got "WARN: Cannot load the DT" followed by an &amp;lt;INTERRUPT&amp;gt; and linux failed to load.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;Where am I supposed to attach the camera (is CSI0 correct)?&lt;/P&gt;&lt;P&gt;What do I need to add to the build in order access the camera?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 20:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MINISASTOCSI-camera-module-with-i-MX-8QuadMax-MEK-CPU/m-p/1246648#M170933</guid>
      <dc:creator>amberworth</dc:creator>
      <dc:date>2021-03-16T20:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: Using MINISASTOCSI camera module with i.MX 8QuadMax MEK CPU Board (imx8qmmek)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MINISASTOCSI-camera-module-with-i-MX-8QuadMax-MEK-CPU/m-p/1247481#M170996</link>
      <description>&lt;P&gt;I figured out what the problem was, I was trying to use the wrong device tree file.&amp;nbsp; I changed it to&amp;nbsp;&lt;/P&gt;&lt;P&gt;setenv &lt;SPAN&gt;fdt_file&amp;nbsp;&lt;/SPAN&gt;imx8qm-mek-ov5640.dtb&lt;/P&gt;&lt;P&gt;The system then was able to load the camera.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can be closed.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 17:57:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MINISASTOCSI-camera-module-with-i-MX-8QuadMax-MEK-CPU/m-p/1247481#M170996</guid>
      <dc:creator>amberworth</dc:creator>
      <dc:date>2021-03-17T17:57:07Z</dc:date>
    </item>
  </channel>
</rss>