<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Kernel is not loading through NAND boot with IMX6ULL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246875#M170957</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the ddr&amp;nbsp;&lt;SPAN&gt;coefficients&lt;/SPAN&gt; already updated once during DRAM bring-up.&lt;/P&gt;&lt;P&gt;And I see for net-boot is booting fine with the same addresses set as for the NAND boot for kernel and dtb files as below,&lt;/P&gt;&lt;P&gt;Loading file 'zImage-imx6ull.bin' to addr 0x80800000...&lt;BR /&gt;Done&lt;BR /&gt;Loading file 'imx6ull-14x14' to addr 0x83000000...&lt;BR /&gt;Done&lt;/P&gt;&lt;P&gt;What impact that could have on different kind of booting methods?&lt;/P&gt;&lt;P&gt;Do you see any other relevant area to review?&lt;/P&gt;&lt;P&gt;-Kiran&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Mar 2021 06:22:34 GMT</pubDate>
    <dc:creator>kmagi</dc:creator>
    <dc:date>2021-03-17T06:22:34Z</dc:date>
    <item>
      <title>Kernel is not loading through NAND boot with IMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246820#M170946</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am looking for some help as I am facing issue in loading kernel through nand boot. The nand boot is stuck after the last log message "Starting kernel ..."&lt;/P&gt;&lt;P&gt;Please find the logs below,&lt;/P&gt;&lt;P&gt;U-Boot 2020.04-imx_v2020.04_5.4.24_2.1.0+g4979a99482 (Mar 15 2021 - 13:08:31 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX6ULL rev1.1 792 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 36C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;NAND: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from NAND... OK&lt;BR /&gt;Display: XXXXXXX-QVGA (480x320)&lt;BR /&gt;Video: 480x320x24&lt;BR /&gt;Error: no valid bmp image at 8c000000&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@2188000 (eth0) using random MAC address - 46:11:08:1d:40:fc&lt;BR /&gt;eth0: ethernet@2188000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Booting from NAND ...&lt;BR /&gt;ubi0: attaching mtd2&lt;BR /&gt;ubi0: scanning is finished&lt;BR /&gt;ubi0: attached mtd2 (name "ubi-part", size 504 MiB)&lt;BR /&gt;ubi0: PEB size: 262144 bytes (256 KiB), LEB size: 253952 bytes&lt;BR /&gt;ubi0: min./max. I/O unit sizes: 4096/4096, sub-page size 4096&lt;BR /&gt;ubi0: VID header offset: 4096 (aligned 4096), data offset: 8192&lt;BR /&gt;ubi0: good PEBs: 2016, bad PEBs: 0, corrupted PEBs: 0&lt;BR /&gt;ubi0: user volume: 5, internal volumes: 1, max. volumes count: 128&lt;BR /&gt;ubi0: max/mean erase counter: 2/1, WL threshold: 4096, image sequence number: 1262705227&lt;BR /&gt;ubi0: available PEBs: 0, total reserved PEBs: 2016, PEBs reserved for bad PEB handling: 40&lt;BR /&gt;Loading file 'zImage-imx6ull.bin' to addr 0x80800000...&lt;BR /&gt;Done&lt;BR /&gt;Loading file 'imx6ull-14x14.dtb' to addr 0x83000000...&lt;BR /&gt;Done&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x5db0c0 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 83000000, end 8300abb0&lt;BR /&gt;Modify /soc/aips-bus@02200000/epdc@0228c000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Same images when I do netboot, works well,&lt;/P&gt;&lt;P&gt;=&amp;gt; run netboot&lt;BR /&gt;Booting from net ...&lt;BR /&gt;Using ethernet@2188000 device&lt;BR /&gt;TFTP from server 192.168.1.7; our IP address is 192.168.1.2&lt;BR /&gt;Filename 'zImage-imx6ull-everett-p1.bin'.&lt;BR /&gt;Load address: 0x80800000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#############################&lt;BR /&gt;854.5 KiB/s&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 6140096 (5db0c0 hex)&lt;BR /&gt;Using ethernet@2188000 device&lt;BR /&gt;TFTP from server 192.168.1.7; our IP address is 192.168.1.2&lt;BR /&gt;Filename 'imx6ull-14x14-everett.dtb'.&lt;BR /&gt;Load address: 0x83000000&lt;BR /&gt;Loading: ###&lt;BR /&gt;702.1 KiB/s&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 31665 (7bb1 hex)&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x5db0c0 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 83000000, end 8300abb0&lt;BR /&gt;Modify /soc/aips-bus@02200000/epdc@0228c000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.14.98-imx+g1175b5961153 (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Wed Mar 10 00:24:42 UTC 2021&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: div instructions available: patching division code&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;OF: fdt: Machine model: Freescale i.MX6 ULL 14x14 Everett Board&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;Reserved memory: created CMA memory pool at 0x8c000000, size 64 MiB&lt;BR /&gt;OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;percpu: Embedded 15 pages/cpu @8bdb2000 s31436 r8192 d21812 u61440&lt;BR /&gt;Built 1 zonelists, mobility grouping on. Total pages: 65024&lt;BR /&gt;Kernel command line: console=ttymxc1 cmdlinepart.mtdparts=gpmi-nand:4m(u-boot),504m(ubi-part),2m(life-data),-(mfg) root=/dev/nfs ip=dhcp nfsroot=192.168.1.7:/nfsroot,v3,tcp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are some environment variable details I am sharing,&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc1,115200 rdinit=/linuxrc clk_ignore_unused&lt;BR /&gt;bootcmd=echo Booting from NAND ...;run mybootargs-1; ubi part ubi-part &amp;amp;&amp;amp; ubifsmount ubi0:kernel1 &amp;amp;&amp;amp; ubifsload ${loadaddr} ${image} &amp;amp;&amp;amp; ubifsload ${fdt_addr} ${fdt_file}; bootz ${loadaddr} - ${fdt_addr};&lt;/P&gt;&lt;P&gt;mtdparts=mtdparts=gpmi-nand:4m(u-boot),504m(ubi-part),2m(life-data),-(mfg)&lt;BR /&gt;mybootargs-1=setenv bootargs console=${console} cmdlinepart.${mtdparts} ${optargs} mem=512M rootwait=1 ro ubi.mtd=ubi-part ubi.block=0,1 rootfstype=squashfs root=/dev/ubiblock0_1 ip=none&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kiran&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 03:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246820#M170946</guid>
      <dc:creator>kmagi</dc:creator>
      <dc:date>2021-03-17T03:56:48Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel is not loading through NAND boot with IMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246833#M170948</link>
      <description>&lt;P&gt;Hi Kiran&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to run ddr test&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/1108221" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/1108221&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and update uboot dcd header with new ddr coefficients found from test&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6ullevk/imximage.cfg?h=imx_v2020.04_5.4.24_2.1.0" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6ullevk/imximage.cfg?h=imx_v2020.04_5.4.24_2.1.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;then program image to nand using uuu tool&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXPmicro/mfgtools" target="_blank" rel="noopener"&gt;https://github.com/NXPmicro/mfgtools&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Technology-Days-Training/i-MX-8-Universal-Update-Utility-UUU-Tools-and-Pins-Tool/ta-p/1129339" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Technology-Days-Training/i-MX-8-Universal-Update-Utility-UUU-Tools-and-Pins-Tool/ta-p/1129339&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also from log : U-Boot 2020.04-imx_v2020.04_5.4.24_2.1.0 - for that uboot recommended to use L5.4.24_2.1.0, not&lt;/P&gt;
&lt;P&gt;Linux version 4.14.98.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 04:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246833#M170948</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-17T04:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel is not loading through NAND boot with IMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246875#M170957</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the ddr&amp;nbsp;&lt;SPAN&gt;coefficients&lt;/SPAN&gt; already updated once during DRAM bring-up.&lt;/P&gt;&lt;P&gt;And I see for net-boot is booting fine with the same addresses set as for the NAND boot for kernel and dtb files as below,&lt;/P&gt;&lt;P&gt;Loading file 'zImage-imx6ull.bin' to addr 0x80800000...&lt;BR /&gt;Done&lt;BR /&gt;Loading file 'imx6ull-14x14' to addr 0x83000000...&lt;BR /&gt;Done&lt;/P&gt;&lt;P&gt;What impact that could have on different kind of booting methods?&lt;/P&gt;&lt;P&gt;Do you see any other relevant area to review?&lt;/P&gt;&lt;P&gt;-Kiran&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 06:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246875#M170957</guid>
      <dc:creator>kmagi</dc:creator>
      <dc:date>2021-03-17T06:22:34Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel is not loading through NAND boot with IMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246953#M170964</link>
      <description>&lt;DIV id="bodyDisplay_0" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;Hi Kiran&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in general for each linux release one can look at Linux Guide document, for example&lt;/P&gt;
&lt;P&gt;Table 1. Image layout, Table 53. Board-specific default values&lt;/P&gt;
&lt;P&gt;&lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_blank" rel="noopener"&gt;i.MX Linux User’s Guide​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 17 Mar 2021 07:55:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1246953#M170964</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-17T07:55:15Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel is not loading through NAND boot with IMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1248465#M171090</link>
      <description>&lt;P&gt;Sorted out the problem&lt;/P&gt;&lt;P&gt;My boot args were wrong&lt;/P&gt;&lt;P&gt;mybootargs-1=setenv bootargs console=${console} cmdlinepart.${mtdparts} ${optargs} mem=512M rootwait=1 ro ubi.mtd=ubi-part ubi.block=0,1 rootfstype=squashfs root=/dev/ubiblock0_1 ip=none&lt;/P&gt;&lt;P&gt;The mem size set was 512M whereas, my DRAM size is just 256M.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 01:03:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-is-not-loading-through-NAND-boot-with-IMX6ULL/m-p/1248465#M171090</guid>
      <dc:creator>kmagi</dc:creator>
      <dc:date>2021-03-19T01:03:48Z</dc:date>
    </item>
  </channel>
</rss>