<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Technical Support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Technical-Support/m-p/1246343#M170911</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184530"&gt;@priyadarshini_m&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;From i.MX 8M Mini LPDDR4 EVKB Board Hardware User's Guide( Rev. 0, February 18, 2021):&lt;BR /&gt;&lt;BR /&gt;2.19 (User interface buttons)&lt;BR /&gt;&lt;BR /&gt;There are two user interface buttons on the EVKB board.&lt;/P&gt;
&lt;P&gt;2.19.1 [Power button (SW901)]&lt;BR /&gt;&lt;BR /&gt;The i.MX 8M Mini Applications Processor supports the use of a button input signal to request main SoC power state changes (i.e. ON or OFF) from the PMU.&lt;BR /&gt;The ON/OFF button can be used for debounce, OFF-to-ON time, and max timeout. Debounce is used to generate the power-off interrupt. In the ON state, if the ON/OFF button is held longer than the debounce time, the power-off interrupt is generated. In the OFF state, if the ON/OFF button is held longer than the OFF-to-ON time, the state will transit from OFF to ON. Max timeout can also be the time for requesting physical power down after the ON/OFF button has been held for the defined time.&lt;/P&gt;
&lt;P&gt;2.19.2 [Reset button (SW902)]&lt;BR /&gt;&lt;BR /&gt;The RESET button (SW902) is directly connected to the PMIC PCA9450A. Holding the RESET button will force to reset the PMIC power outputs except NVCC_SNVS_1V8 and VDD_SNVS_0V8 on the EVKB board. The i.MX 8M Mini applications processor will be immediately turned off and reinitiate a boot cycle from the OFF state.&lt;BR /&gt;&lt;BR /&gt;&amp;lt; &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX8MMEVKBHUG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX8MMEVKBHUG.pdf&lt;/A&gt; &amp;gt;&lt;/P&gt;
&lt;P&gt;According to Hardware Development Guide for the i.MX8Mm:&lt;BR /&gt;&lt;BR /&gt;For portable applications, the ONOFF pin may be connected to an ON/OFF SPST push-button switch to ground.&amp;nbsp; An external pull-up resistor is required on this pin.&lt;/P&gt;
&lt;P&gt;A brief connection to GND in OFF mode causes the internal power management state machine to change state to ON.&amp;nbsp; In ON mode, a brief connection to GND generates an interrupt (intended to initiate a software-controllable&amp;nbsp; power-down). The connection to GND for approximate 5 seconds or more causes a forced OFF.&lt;/P&gt;
&lt;P&gt;&amp;lt; &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX8MMHDG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX8MMHDG.pdf&lt;/A&gt; &amp;gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 10:09:26 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2021-03-16T10:09:26Z</dc:date>
    <item>
      <title>Technical Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Technical-Support/m-p/1246257#M170907</link>
      <description>Kindly clarify power on reset for IMX8M Mini application processor.. When I press the reset button, then how much time delay needed so that the power on reset pin will detect the signal and get enabled?</description>
      <pubDate>Tue, 16 Mar 2021 08:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Technical-Support/m-p/1246257#M170907</guid>
      <dc:creator>priyadarshini_m</dc:creator>
      <dc:date>2021-03-16T08:38:43Z</dc:date>
    </item>
    <item>
      <title>Re: Technical Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Technical-Support/m-p/1246343#M170911</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184530"&gt;@priyadarshini_m&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;From i.MX 8M Mini LPDDR4 EVKB Board Hardware User's Guide( Rev. 0, February 18, 2021):&lt;BR /&gt;&lt;BR /&gt;2.19 (User interface buttons)&lt;BR /&gt;&lt;BR /&gt;There are two user interface buttons on the EVKB board.&lt;/P&gt;
&lt;P&gt;2.19.1 [Power button (SW901)]&lt;BR /&gt;&lt;BR /&gt;The i.MX 8M Mini Applications Processor supports the use of a button input signal to request main SoC power state changes (i.e. ON or OFF) from the PMU.&lt;BR /&gt;The ON/OFF button can be used for debounce, OFF-to-ON time, and max timeout. Debounce is used to generate the power-off interrupt. In the ON state, if the ON/OFF button is held longer than the debounce time, the power-off interrupt is generated. In the OFF state, if the ON/OFF button is held longer than the OFF-to-ON time, the state will transit from OFF to ON. Max timeout can also be the time for requesting physical power down after the ON/OFF button has been held for the defined time.&lt;/P&gt;
&lt;P&gt;2.19.2 [Reset button (SW902)]&lt;BR /&gt;&lt;BR /&gt;The RESET button (SW902) is directly connected to the PMIC PCA9450A. Holding the RESET button will force to reset the PMIC power outputs except NVCC_SNVS_1V8 and VDD_SNVS_0V8 on the EVKB board. The i.MX 8M Mini applications processor will be immediately turned off and reinitiate a boot cycle from the OFF state.&lt;BR /&gt;&lt;BR /&gt;&amp;lt; &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX8MMEVKBHUG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX8MMEVKBHUG.pdf&lt;/A&gt; &amp;gt;&lt;/P&gt;
&lt;P&gt;According to Hardware Development Guide for the i.MX8Mm:&lt;BR /&gt;&lt;BR /&gt;For portable applications, the ONOFF pin may be connected to an ON/OFF SPST push-button switch to ground.&amp;nbsp; An external pull-up resistor is required on this pin.&lt;/P&gt;
&lt;P&gt;A brief connection to GND in OFF mode causes the internal power management state machine to change state to ON.&amp;nbsp; In ON mode, a brief connection to GND generates an interrupt (intended to initiate a software-controllable&amp;nbsp; power-down). The connection to GND for approximate 5 seconds or more causes a forced OFF.&lt;/P&gt;
&lt;P&gt;&amp;lt; &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX8MMHDG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX8MMHDG.pdf&lt;/A&gt; &amp;gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 10:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Technical-Support/m-p/1246343#M170911</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-03-16T10:09:26Z</dc:date>
    </item>
  </channel>
</rss>