<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX 8M mini processor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-mini-processor/m-p/1244658#M170761</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;In our design if we are not using a NOR flash like done in EVK board for iMX 8M mini, what to do with the NAND interface PINS used for FLASH connectivity?&lt;/P&gt;&lt;P&gt;Shall we leave them unconnected, no such guide is present in IMX8MMHDG,please recommend usage&lt;/P&gt;&lt;P&gt;Also, CLKIN1, CLKIN2, CLKOUT1, CLKOUT2, is there any clock signal available there, what is the frequency, can we use it to clock some other peripheral device?&lt;/P&gt;&lt;P&gt;Standalone SOM board can support eMMC/SDHC3 boot, by populating R71, R72, R75, R76, R79, R95, R97! Can this be used to boot from eMMC directly without setting the boot switches SW1101 &amp;amp; SW1102 or without the baseboard, any documentation on this&lt;/P&gt;&lt;P&gt;Please write back,&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;</description>
    <pubDate>Fri, 12 Mar 2021 07:17:17 GMT</pubDate>
    <dc:creator>pantarun_92</dc:creator>
    <dc:date>2021-03-12T07:17:17Z</dc:date>
    <item>
      <title>iMX 8M mini processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-mini-processor/m-p/1244658#M170761</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;In our design if we are not using a NOR flash like done in EVK board for iMX 8M mini, what to do with the NAND interface PINS used for FLASH connectivity?&lt;/P&gt;&lt;P&gt;Shall we leave them unconnected, no such guide is present in IMX8MMHDG,please recommend usage&lt;/P&gt;&lt;P&gt;Also, CLKIN1, CLKIN2, CLKOUT1, CLKOUT2, is there any clock signal available there, what is the frequency, can we use it to clock some other peripheral device?&lt;/P&gt;&lt;P&gt;Standalone SOM board can support eMMC/SDHC3 boot, by populating R71, R72, R75, R76, R79, R95, R97! Can this be used to boot from eMMC directly without setting the boot switches SW1101 &amp;amp; SW1102 or without the baseboard, any documentation on this&lt;/P&gt;&lt;P&gt;Please write back,&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;</description>
      <pubDate>Fri, 12 Mar 2021 07:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-mini-processor/m-p/1244658#M170761</guid>
      <dc:creator>pantarun_92</dc:creator>
      <dc:date>2021-03-12T07:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 8M mini processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-mini-processor/m-p/1244746#M170772</link>
      <description>&lt;P&gt;Hi Arun&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt; if we are not using a NOR flash like done in EVK board for iMX 8M mini,&lt;/P&gt;
&lt;P&gt;&amp;gt;what to do with the NAND interface PINS used for FLASH connectivity?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;they can be left unconnected.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt; CLKIN1, CLKIN2, CLKOUT1, CLKOUT2, is there any clock signal available there&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;these clocks are programmable, description can be found in sect.5.1.8.38 PLL Clock Output for Test Enable and Select Register (CCM_ANALOG_ANAMIX_PLL_MNIT_CTL)&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX8MMRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Mini Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Can this be used to boot from eMMC directly without setting the boot switches SW1101 &amp;amp; SW1102&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;not sorry.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 12 Mar 2021 09:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-mini-processor/m-p/1244746#M170772</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-12T09:44:13Z</dc:date>
    </item>
  </channel>
</rss>