<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx8qm flexcan bus error at board side in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8qm-flexcan-bus-error-at-board-side/m-p/1244578#M170754</link>
    <description>&lt;P&gt;hello I am using the i.mx8qm MEK board for adas project&lt;/P&gt;&lt;P&gt;as per the procedure provided in the below link&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-management-service/ta-p/1123227" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-management-service/ta-p/1123227&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did the image build now can communication is working but the issue is if the &lt;STRONG&gt;first message sends from the board that time can bus is in an off state (error counter is also zero).&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;But if the first message sent from another node or host pc that time can communication working without any issue, can bus working fine&lt;/P&gt;&lt;P&gt;any idea regarding this behavior??????&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 12 Mar 2021 05:09:49 GMT</pubDate>
    <dc:creator>aksh9354</dc:creator>
    <dc:date>2021-03-12T05:09:49Z</dc:date>
    <item>
      <title>i.mx8qm flexcan bus error at board side</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8qm-flexcan-bus-error-at-board-side/m-p/1244578#M170754</link>
      <description>&lt;P&gt;hello I am using the i.mx8qm MEK board for adas project&lt;/P&gt;&lt;P&gt;as per the procedure provided in the below link&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-management-service/ta-p/1123227" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-management-service/ta-p/1123227&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did the image build now can communication is working but the issue is if the &lt;STRONG&gt;first message sends from the board that time can bus is in an off state (error counter is also zero).&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;But if the first message sent from another node or host pc that time can communication working without any issue, can bus working fine&lt;/P&gt;&lt;P&gt;any idea regarding this behavior??????&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Mar 2021 05:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8qm-flexcan-bus-error-at-board-side/m-p/1244578#M170754</guid>
      <dc:creator>aksh9354</dc:creator>
      <dc:date>2021-03-12T05:09:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8qm flexcan bus error at board side</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8qm-flexcan-bus-error-at-board-side/m-p/1245205#M170817</link>
      <description>&lt;P&gt;Hi aksh9354&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can check if both sides use similar mode, can or can-fd. Example for legacy mode&lt;/P&gt;
&lt;P&gt;with "disable-fd-mode" can be found on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/alliedvision/linux_imx8_apalis/blob/master/arch/arm64/boot/dts/freescale/fsl-imx8qm-apalis.dts" target="_blank"&gt;https://github.com/alliedvision/linux_imx8_apalis/blob/master/arch/arm64/boot/dts/freescale/fsl-imx8qm-apalis.dts&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also may be recommended to try to reproduce issue using two MEK boards and latest&lt;/P&gt;
&lt;P&gt;nxp linux from source.codeaurora.org/external/imx/linux-imx repository&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.70_2.3.0" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Documentation&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Then try to debug issue using AN12631&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_7" href="https://www.nxp.com/docs/en/application-note/AN12631.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;Normal and Secure Debug for i.MX8/8X Family of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 14 Mar 2021 09:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8qm-flexcan-bus-error-at-board-side/m-p/1245205#M170817</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-14T09:37:58Z</dc:date>
    </item>
  </channel>
</rss>