<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8m M4 GPIO_PinInit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-M4-GPIO-PinInit/m-p/1239496#M170298</link>
    <description>&lt;P&gt;I am using rproc to load an image running FreeRTOS into the m4 and run.&lt;/P&gt;&lt;P&gt;The M4 uses GPIO_PinInit to setup SPI and gpio interrupts.&lt;/P&gt;&lt;P&gt;We also use some scripts on the Linux side to configure IO pins.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can the M4 call GPIO_PinInit at anytime or do we need to be concerned about when the M4 calls these functions if Linux is configuring IO (for different pins) at the same time?&lt;/P&gt;</description>
    <pubDate>Wed, 03 Mar 2021 16:55:18 GMT</pubDate>
    <dc:creator>lmcbeath</dc:creator>
    <dc:date>2021-03-03T16:55:18Z</dc:date>
    <item>
      <title>imx8m M4 GPIO_PinInit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-M4-GPIO-PinInit/m-p/1239496#M170298</link>
      <description>&lt;P&gt;I am using rproc to load an image running FreeRTOS into the m4 and run.&lt;/P&gt;&lt;P&gt;The M4 uses GPIO_PinInit to setup SPI and gpio interrupts.&lt;/P&gt;&lt;P&gt;We also use some scripts on the Linux side to configure IO pins.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can the M4 call GPIO_PinInit at anytime or do we need to be concerned about when the M4 calls these functions if Linux is configuring IO (for different pins) at the same time?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 16:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-M4-GPIO-PinInit/m-p/1239496#M170298</guid>
      <dc:creator>lmcbeath</dc:creator>
      <dc:date>2021-03-03T16:55:18Z</dc:date>
    </item>
  </channel>
</rss>