<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDDR test, not understanding a parameter</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-test-not-understanding-a-parameter/m-p/1239484#M170297</link>
    <description>&lt;P&gt;Hi and good day,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the IMX6DL&amp;nbsp; with&amp;nbsp;MT41K128M16JT-125 from Micron on one of our boards. The memory is a 2GB DDR3 128M x 16 x 8bank; 14 row addresses, 10 column addresses and we are using 4 of them with 1 CS to cover all 64 data lines.&lt;/P&gt;&lt;P&gt;When I enter those parameter into the DDR test, I received back that the DDR Density per Chip Select is 1024MB. I have the DDR density selection to Default but I can't change it. Why does it not shows 2048MB?&lt;/P&gt;&lt;P&gt;Also, when I run the SSR Stress Test it usually fails at the first frequency. But if I change the DDR Density for 512MB in the drop down menu (also need to update the data bus to 32 bits) I can run the calibration as well as the DDR Stress test without any issues.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there something I don't see/understand here?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Fred_Jutras_0-1614788670804.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138625iDCC462789AB9C42B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Fred_Jutras_0-1614788670804.png" alt="Fred_Jutras_0-1614788670804.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Fred_Jutras_0-1614788670804.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Fred_Jutras_0-1614788982426.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138626iBAC52EF42A21ED26/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Fred_Jutras_0-1614788982426.png" alt="Fred_Jutras_0-1614788982426.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Fred_Jutras_0-1614788982426.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR Stress Test (3.0.0)&lt;BR /&gt;Build: Dec 14 2018, 14:12:28&lt;BR /&gt;NXP Semiconductors.&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Solo/DualLite (0x61)&lt;BR /&gt;Internal Revision = TO1.3&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00007040&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x29000001&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3&lt;BR /&gt;Data width: 64, bank num: 8&lt;BR /&gt;Row size: 14, col size: 10&lt;BR /&gt;Chip select CSD0 is used&lt;BR /&gt;Density per chip select: 1024MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
    <pubDate>Wed, 03 Mar 2021 16:29:50 GMT</pubDate>
    <dc:creator>Fred_Jutras</dc:creator>
    <dc:date>2021-03-03T16:29:50Z</dc:date>
    <item>
      <title>DDR test, not understanding a parameter</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-test-not-understanding-a-parameter/m-p/1239484#M170297</link>
      <description>&lt;P&gt;Hi and good day,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the IMX6DL&amp;nbsp; with&amp;nbsp;MT41K128M16JT-125 from Micron on one of our boards. The memory is a 2GB DDR3 128M x 16 x 8bank; 14 row addresses, 10 column addresses and we are using 4 of them with 1 CS to cover all 64 data lines.&lt;/P&gt;&lt;P&gt;When I enter those parameter into the DDR test, I received back that the DDR Density per Chip Select is 1024MB. I have the DDR density selection to Default but I can't change it. Why does it not shows 2048MB?&lt;/P&gt;&lt;P&gt;Also, when I run the SSR Stress Test it usually fails at the first frequency. But if I change the DDR Density for 512MB in the drop down menu (also need to update the data bus to 32 bits) I can run the calibration as well as the DDR Stress test without any issues.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there something I don't see/understand here?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Fred_Jutras_0-1614788670804.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138625iDCC462789AB9C42B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Fred_Jutras_0-1614788670804.png" alt="Fred_Jutras_0-1614788670804.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Fred_Jutras_0-1614788670804.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Fred_Jutras_0-1614788982426.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138626iBAC52EF42A21ED26/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Fred_Jutras_0-1614788982426.png" alt="Fred_Jutras_0-1614788982426.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Fred_Jutras_0-1614788982426.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR Stress Test (3.0.0)&lt;BR /&gt;Build: Dec 14 2018, 14:12:28&lt;BR /&gt;NXP Semiconductors.&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Solo/DualLite (0x61)&lt;BR /&gt;Internal Revision = TO1.3&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00007040&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x29000001&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3&lt;BR /&gt;Data width: 64, bank num: 8&lt;BR /&gt;Row size: 14, col size: 10&lt;BR /&gt;Chip select CSD0 is used&lt;BR /&gt;Density per chip select: 1024MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 16:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-test-not-understanding-a-parameter/m-p/1239484#M170297</guid>
      <dc:creator>Fred_Jutras</dc:creator>
      <dc:date>2021-03-03T16:29:50Z</dc:date>
    </item>
  </channel>
</rss>