<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Frame Syncs are not in Phase in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1239104#M170261</link>
    <description>&lt;P&gt;Hi Sreedhar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay&lt;/P&gt;
&lt;P&gt;(there is no such hardware settings in SAI module), sorry.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Wed, 03 Mar 2021 05:46:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-03-03T05:46:00Z</dc:date>
    <item>
      <title>Frame Syncs are not in Phase</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1238904#M170232</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with i.MX8MM EVK and another SoC is interfaced to the EVK hw.&lt;/P&gt;&lt;P&gt;The SAI1 of iMX8MM is Master and generating the Frame Sync.&lt;/P&gt;&lt;P&gt;This Frame Sync from SAI1 is connected to I2S In Port of SoC.&lt;/P&gt;&lt;P&gt;Internally in SoC this Frame Sync is routed to I2S Out port and it is used as Frame Sync of I2S Out&lt;/P&gt;&lt;P&gt;When we observe these two Frame Syncs (Frame Sync Generated by SAI1 and Frame Sync at I2S Out port) on CRO. they are not in phase.&lt;/P&gt;&lt;P&gt;Is there a way or any programming sequence of SAI registers can we achieve the similar phase?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because out of phase can lead us to sample swap issues.&lt;/P&gt;&lt;P&gt;Please let us know.&lt;/P&gt;&lt;P&gt;Thank you, Sreedhar&lt;/P&gt;</description>
      <pubDate>Tue, 02 Mar 2021 22:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1238904#M170232</guid>
      <dc:creator>sreedhar_appala</dc:creator>
      <dc:date>2021-03-02T22:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: Frame Syncs are not in Phase</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1239104#M170261</link>
      <description>&lt;P&gt;Hi Sreedhar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay&lt;/P&gt;
&lt;P&gt;(there is no such hardware settings in SAI module), sorry.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 05:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1239104#M170261</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-03T05:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: Frame Syncs are not in Phase</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1239115#M170262</link>
      <description>&lt;P&gt;Thank you Igor !!&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 06:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-Syncs-are-not-in-Phase/m-p/1239115#M170262</guid>
      <dc:creator>sreedhar_appala</dc:creator>
      <dc:date>2021-03-03T06:16:34Z</dc:date>
    </item>
  </channel>
</rss>