<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Query on the Tamper Pin in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1238594#M170209</link>
    <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;There are total 10 tamper pins together in the application processor which i am using.&lt;/P&gt;&lt;P&gt;I am planning to use only two pins a tamper, other pins as the GPIO's.&lt;/P&gt;&lt;P&gt;It is mentioned like this in the datasheet for the power section of tamper pins.&lt;/P&gt;&lt;P&gt;" VDD_TMPR_CSI_1P8_3P3 Shall be connected to VDD_SNVS_LDO_1P8_CAP when used as a&lt;BR /&gt;tamper pin. In CSI mode use an external 1.8 V supply. In this case, follow the 1.8 VI/O specification above."&lt;/P&gt;&lt;P&gt;If i want to use the above case ( i.e two as a tamper pin &amp;amp; other as GPIO) what should be the power domain to&amp;nbsp;VDD_TMPR_CSI_1P8_3P3.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 02 Mar 2021 09:27:55 GMT</pubDate>
    <dc:creator>puneethkumar</dc:creator>
    <dc:date>2021-03-02T09:27:55Z</dc:date>
    <item>
      <title>Query on the Tamper Pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1238594#M170209</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;There are total 10 tamper pins together in the application processor which i am using.&lt;/P&gt;&lt;P&gt;I am planning to use only two pins a tamper, other pins as the GPIO's.&lt;/P&gt;&lt;P&gt;It is mentioned like this in the datasheet for the power section of tamper pins.&lt;/P&gt;&lt;P&gt;" VDD_TMPR_CSI_1P8_3P3 Shall be connected to VDD_SNVS_LDO_1P8_CAP when used as a&lt;BR /&gt;tamper pin. In CSI mode use an external 1.8 V supply. In this case, follow the 1.8 VI/O specification above."&lt;/P&gt;&lt;P&gt;If i want to use the above case ( i.e two as a tamper pin &amp;amp; other as GPIO) what should be the power domain to&amp;nbsp;VDD_TMPR_CSI_1P8_3P3.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Mar 2021 09:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1238594#M170209</guid>
      <dc:creator>puneethkumar</dc:creator>
      <dc:date>2021-03-02T09:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: Query on the Tamper Pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1239325#M170283</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180656"&gt;@puneethkumar&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; connect&amp;nbsp; VDD_TMPR_CSI_1P8_3P3 to VDD_SNVS_LDO_1P8_CAP.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 11:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1239325#M170283</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-03-03T11:23:03Z</dc:date>
    </item>
    <item>
      <title>Re: Query on the Tamper Pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1245370#M170837</link>
      <description>&lt;P&gt;Thanks for the reply&lt;/P&gt;&lt;P&gt;If i make above connection will i able to use tamper pins both as GPIO &amp;amp; tamper detection pins&lt;/P&gt;</description>
      <pubDate>Mon, 15 Mar 2021 05:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1245370#M170837</guid>
      <dc:creator>puneethkumar</dc:creator>
      <dc:date>2021-03-15T05:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: Query on the Tamper Pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1245478#M170844</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180656"&gt;@puneethkumar&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; It is recommended to use VDD_SNVS_LDO_1P8_CAP as voltage source &lt;BR /&gt;for the tamper pins in order to be able to detect tampers in low power modes.&lt;BR /&gt;&amp;nbsp;If there are not requirements to detect events in low power modes, any &lt;BR /&gt;voltage source may be applied.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Mar 2021 07:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-the-Tamper-Pin/m-p/1245478#M170844</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-03-15T07:34:07Z</dc:date>
    </item>
  </channel>
</rss>