<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6SLL boot config</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-boot-config/m-p/1238204#M170171</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm on a custom board with a IMX6SLL chip.&lt;/P&gt;&lt;P&gt;I'm debugging using a JTAG link and would like to change the boot configuration through the JTAG port.&lt;/P&gt;&lt;P&gt;I want to use the SD card as the boot device, but I don't have access to the LCD_GPIOs used to override the BOOT_CFG signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I use the JTAG to change the booting configuration and set the SD card as the boot device? What registers should I modified to achieve it? And what address should I point to reboot the chip using the new config?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Vincent&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 21:40:58 GMT</pubDate>
    <dc:creator>vlintilhac</dc:creator>
    <dc:date>2021-03-01T21:40:58Z</dc:date>
    <item>
      <title>IMX6SLL boot config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-boot-config/m-p/1238204#M170171</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm on a custom board with a IMX6SLL chip.&lt;/P&gt;&lt;P&gt;I'm debugging using a JTAG link and would like to change the boot configuration through the JTAG port.&lt;/P&gt;&lt;P&gt;I want to use the SD card as the boot device, but I don't have access to the LCD_GPIOs used to override the BOOT_CFG signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I use the JTAG to change the booting configuration and set the SD card as the boot device? What registers should I modified to achieve it? And what address should I point to reboot the chip using the new config?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Vincent&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 21:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-boot-config/m-p/1238204#M170171</guid>
      <dc:creator>vlintilhac</dc:creator>
      <dc:date>2021-03-01T21:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SLL boot config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-boot-config/m-p/1238256#M170174</link>
      <description>&lt;P&gt;Hi Vincent&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in general boot configuration is latched at POR in SRC_SBMR1, SRC_SBMR2 registers&lt;/P&gt;
&lt;P&gt;(read only),described in sect.41.7.2 SRC Boot Mode Register 1 (SRC_SBMR1)&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX6SLLRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6SLL Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;so seems it is not possible to use jtag for changing the booting configuration.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 23:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-boot-config/m-p/1238256#M170174</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-03-01T23:15:33Z</dc:date>
    </item>
  </channel>
</rss>